Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Newbie - need a simple SIP package
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 1158 views
  • Users 0 members are here
Related

Newbie - need a simple SIP package

e14 Contributor
e14 Contributor over 14 years ago

I'm new to Eagle and have a need to create a simple board.  I believe I can figure out how to do most of the layout but one of my parts is an uncommon part with a single inline package with standard hole spacing (same as a prototyping board.)  I've spent a lot of time reading instructions and viewing tutorials but am still not understanding a straightforward way to modify an existing package to do what I need.  My electronic part is a an RF receiver board about 2" long with 8 pins at various points and looks like this:

 

http://gallery.mac.com/swearingendw#100075/IMG_3552&bgcolor=black

 

Ideally I could just grab an existing package and remove a few of the pins and be good to go.

 

Can anyone explain for me in clear steps how I might do this or whatever it takes to get this into Eagle?

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Am 11.09.2011 16:59, schrieb bethesdaboys:

    I'm new to Eagle and have a need to create a simple board.  I believe I can figure out how to do most of the layout but one of my parts is an uncommon part with a single inline package with standard hole spacing (same as a prototyping board.)  I've spent a lot of time reading instructions and viewing tutorials but am still not understanding a straightforward way to modify an existing package to do what I need.  My electronic part is a an RF receiver board about 2" long with 8 pins at various points and looks like this:

     

    http://gallery.mac.com/swearingendw#100075/IMG_3552&bgcolor=black

     

    Ideally I could just grab an existing package and remove a few of the pins and be good to go.

     

    Can anyone explain for me in clear steps how I might do this or whatever it takes to get this into Eagle?

     

    Thanks!

     

     

    What you need is a library for your part. Since

    you say it's a sil package I attached a library SIL.lbr which I

    generated from resistor-sil.lbr.You must open the library and edit it to

    fit your needs. Tutorials how to edit eagle libraries can be found in

    the internet and in the eagle doc-directory.

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thank you Joern!

     

    However I do not see an attachment to your post.

     

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I cannot see an attachment either, some people seems to have access into element14 by usernet. Unfortunaetly it doesnt work well. To edit package in library: 1. be sure you are in library edit window (you can tell by menu icon apperance, it should be an olive book in contrast to default green board/red-white schematic icons) then select "Library" from main menu and then "Package". Pinheads are located in PINHEAD library, you can find them using "PINHD*". If you are using awesome SparkFun (highly recommend) library look for M components (ex. M2 M5 etc.).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I cannot see an attachment either, some people seems to have access into element14 by usernet. Unfortunaetly it doesnt work well. To edit package in library: 1. be sure you are in library edit window (you can tell by menu icon apperance, it should be an olive book in contrast to default green board/red-white schematic icons) then select "Library" from main menu and then "Package". Pinheads are located in PINHEAD library, you can find them using "PINHD*". If you are using awesome SparkFun (highly recommend) library look for M components (ex. M2 M5 etc.).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 11.09.2011 20:46, schrieb Maciej Kucia:

    I cannot see an attachment either, some people seems to have access into element14 by usernet. Unfortunaetly it doesnt work well. To edit package in library: 1. be sure you are in library edit window (you can tell by menu icon apperance, it should be an olive book in contrast to default green board/red-white schematic icons) then select "Library" from main menu and then "Package". Pinheads are located in PINHEAD library, you can find them using "PINHD*". If you are using awesome SparkFun (highly recommend) library look for M components (ex. M2 M5 etc.).

     

    From your answer I see that the attachment did not reach the poster.

    Sorry about that. I usually don't check the posters address, just tried

    to help.

    Meanwhile it should be well known that the element14 link does not work

    well. So why not use the eagle central forum or the eagle newsgroup.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag