Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Newbie - need a simple SIP package
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 1178 views
  • Users 0 members are here
Related

Newbie - need a simple SIP package

e14 Contributor
e14 Contributor over 14 years ago

I'm new to Eagle and have a need to create a simple board.  I believe I can figure out how to do most of the layout but one of my parts is an uncommon part with a single inline package with standard hole spacing (same as a prototyping board.)  I've spent a lot of time reading instructions and viewing tutorials but am still not understanding a straightforward way to modify an existing package to do what I need.  My electronic part is a an RF receiver board about 2" long with 8 pins at various points and looks like this:

 

http://gallery.mac.com/swearingendw#100075/IMG_3552&bgcolor=black

 

Ideally I could just grab an existing package and remove a few of the pins and be good to go.

 

Can anyone explain for me in clear steps how I might do this or whatever it takes to get this into Eagle?

 

Thanks!

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 11.09.2011 20:46, schrieb Maciej Kucia:

    I cannot see an attachment either, some people seems to have access into element14 by usernet. Unfortunaetly it doesnt work well. To edit package in library: 1. be sure you are in library edit window (you can tell by menu icon apperance, it should be an olive book in contrast to default green board/red-white schematic icons) then select "Library" from main menu and then "Package". Pinheads are located in PINHEAD library, you can find them using "PINHD*". If you are using awesome SparkFun (highly recommend) library look for M components (ex. M2 M5 etc.).

     

    From your answer I see that the attachment did not reach the poster.

    Sorry about that. I usually don't check the posters address, just tried

    to help.

    Meanwhile it should be well known that the element14 link does not work

    well. So why not use the eagle central forum or the eagle newsgroup.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    bethesdaboys wrote:

    I'm new to Eagle and have a need to create a simple board. I believe

    I can figure out how to do most of the layout but one of my parts is

    an uncommon part with a single inline package with standard hole

    spacing (same as a prototyping board.) I've spent a lot of time

    reading instructions and viewing tutorials but am still not

    understanding a straightforward way to modify an existing package to

    do what I need. My electronic part is a an RF receiver board about 2"

    long with 8 pins at various points and looks like this:

     

    http://gallery.mac.com/swearingendw#100075/IMG_3552&bgcolor=black

     

    Ideally I could just grab an existing package and remove a few of the

    pins and be good to go.

     

    Can anyone explain for me in clear steps how I might do this or

    whatever it takes to get this into Eagle?

     

    Thanks!

     

    Looks like you have one of these

    http://www.sparkfun.com/products/10533

    http://dlnmh9ip6v2uc.cloudfront.net/datasheets/Wireless/General/RWS-374-3_315MHz_ASK_RF_Receiver_Module_Data_Sheet.pdf

     

    There is a package footprint (RF-LINK_RF) in the Sparkfun Eagle library

    https://github.com/sparkfun/SparkFun-Eagle-Library/archives/master

    but don't use it as is. There is an error with it and it needs the pin

    groups seperating by a further 0.1"

    It is for older modules so the tPlace outline may need adjusting to better

    represent the thinkness of your module.

     

    Warren

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I cannot see an attachment either, some people seems to have access into element14 by usernet. Unfortunaetly it doesnt work well. To edit package in library: 1. be sure you are in library edit window (you can tell by menu icon apperance, it should be an olive book in contrast to default green board/red-white schematic icons) then select "Library" from main menu and then "Package". Pinheads are located in PINHEAD library, you can find them using "PINHD*". If you are using awesome SparkFun (highly recommend) library look for M components (ex. M2 M5 etc.).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thank you Joern!

     

    However I do not see an attachment to your post.

     

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Subsequent to posting my message above I remembered that the manual for version 5 states: "Select the Package editing mode via the icon in the action toolbar..." however I do not have this icon/button in my interface or at least I cannot find it.  This was my main problem before.

     

    Thanks for your response, Maciej.  So you're saying use (2) 4-pinhead connectors?  Good idea, but how do I find such a part amongst the thousands of parts?  I search for 'pinhead' and get nothing in the ADD part interface.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Am 11.09.2011 16:59, schrieb bethesdaboys:

    I'm new to Eagle and have a need to create a simple board.  I believe I can figure out how to do most of the layout but one of my parts is an uncommon part with a single inline package with standard hole spacing (same as a prototyping board.)  I've spent a lot of time reading instructions and viewing tutorials but am still not understanding a straightforward way to modify an existing package to do what I need.  My electronic part is a an RF receiver board about 2" long with 8 pins at various points and looks like this:

     

    http://gallery.mac.com/swearingendw#100075/IMG_3552&bgcolor=black

     

    Ideally I could just grab an existing package and remove a few of the pins and be good to go.

     

    Can anyone explain for me in clear steps how I might do this or whatever it takes to get this into Eagle?

     

    Thanks!

     

     

    What you need is a library for your part. Since

    you say it's a sil package I attached a library SIL.lbr which I

    generated from resistor-sil.lbr.You must open the library and edit it to

    fit your needs. Tutorials how to edit eagle libraries can be found in

    the internet and in the eagle doc-directory.

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    There are many tutorials over library creation over Internet. Although if project is simple i would just use 2x 4 pinhead connectors. If you really want to make new element do not use an existing package for such simple task! If you really really want to modify existing package do as follows: open your library, in main eagle window find requested package in some other library and select "copy to library" from context menu. Now part is copied into your library and can be easily modified.

    Hope that will help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer