Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Split Symbol Across Multiple Pages
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 1449 views
  • Users 0 members are here
  • eagle
  • library
  • split
  • schematic
  • symbol
Related

Split Symbol Across Multiple Pages

e14 Contributor
e14 Contributor over 15 years ago

Hello.

I have a device with several hundred pins.  For the sake of organizing my schematic, I'd like to split the library symbol across two pages---I can't easily fit it on to a single page at the moment.  Is this possible in EagleCAD?

 

Any hints or ideas on how to do this (or just make the symbol more manageable) are most appreciated.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    On 09/18/2011 04:03 PM, Ash Charles wrote:

    Hello.

    I have a device with several hundred pins.  For the sake of organizing my schematic, I'd like to split the library symbol across two pages---I can't easily fit it on to a single page at the moment.  Is this possible in EagleCAD?

     

    Any hints or ideas on how to do this (or just make the symbol more manageable) are most appreciated.

     

    On complex IC's, such as microcontrollers, I split the symbols into

    logical blocks.  GPIO A, GPIO B, Power block, JTAG block, USB, EBI, etc.

    for this very purpose.  The only symbol in the device that is marked

    MUST is the power block.  Everything else is marked as CAN.  IN then use

    INVOKE to place the CAN blocks on separate sheets.

     

    DPDT relays are treated the same way.  ADD places the coil, and INVOKE

    places each pole.

     

    Enjoy,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    On 09/18/2011 04:03 PM, Ash Charles wrote:

    Hello.

    I have a device with several hundred pins.  For the sake of organizing my schematic, I'd like to split the library symbol across two pages---I can't easily fit it on to a single page at the moment.  Is this possible in EagleCAD?

     

    Any hints or ideas on how to do this (or just make the symbol more manageable) are most appreciated.

     

    On complex IC's, such as microcontrollers, I split the symbols into

    logical blocks.  GPIO A, GPIO B, Power block, JTAG block, USB, EBI, etc.

    for this very purpose.  The only symbol in the device that is marked

    MUST is the power block.  Everything else is marked as CAN.  IN then use

    INVOKE to place the CAN blocks on separate sheets.

     

    DPDT relays are treated the same way.  ADD places the coil, and INVOKE

    places each pole.

     

    Enjoy,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Thanks---that works like a charm image