Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) USB routing problems : D+/- length issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 30 replies
  • Answers 2 answers
  • Subscribers 191 subscribers
  • Views 3549 views
  • Users 0 members are here
  • length
  • d-
  • autorouter
  • usb
  • parallelism
  • d+
Related

USB routing problems : D+/- length issues

e14 Contributor
e14 Contributor over 14 years ago

Hello everyone

 

I'm a user of Eagle for 2 years now, and i'm trying to make USB with an Overo and a dsPIC.

The thing is that I had read somewhere (http://www.usb.org/developers/docs/hs_usb_pdg_r1_0.pdf) that the signals D+ and D- must have the same length (they talk about non parallelism page 10 figure 5)

 

But here is the point : how you do that on Eagle , to force 2 wire to have the same length (or being parallel all the way), in autorouter mode of course but even in manual mode.

 

Thanks for the help .

 

Best Regards

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Vincent Vittori schrieb:

     

    I'm a user of Eagle for 2 years now, and i'm trying to make USB with

    an Overo and a dsPIC. The thing is that I had read somewhere

    (http://www.usb.org/developers/docs/hs_usb_pdg_r1_0.pdf) that the

    signals D+ and D- must have the same length (they talk about non

    parallelism page 10 figure 5)

     

    But here is the point : how you do that on Eagle , to force 2 wire to

    have the same length (or being parallel all the way), in autorouter

    mode of course but even in manual mode.

     

    First of all, I would never use the autorouter for this. (I don't use it

    at all... but here it's essential.)

     

    Then, simply (manually) route your tracks as parallel as possible. You

    can check their length with an ULP and correct them if necessary.

     

    In EAGLE, there is no way to /force/ an equally long differential pair

    during routing, neither manually nor by autorouter. Maybe V6 will add

    something new here, but I don't know.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kcadsoft
    0 kcadsoft over 14 years ago in reply to e14 Contributor

    On 09/23/11 08:08, Tilmann Reh wrote:

    ...

    In EAGLE, there is no way to /force/ an equally long differential pair

    during routing, neither manually nor by autorouter. Maybe V6 will add

    something new here, but I don't know.

     

    In V6 the (manual) ROUTE command will treat signals that have the

    same net class and the same name (one ending with '+' and the other

    with '-') as "differential pairs". When picking up one airwire of such

    a pair, both signals will be routed in parallel, keeping the distance

    as defined in the net class.

     

    This can't guarantee the same length for both signals, so there

    will also be a new command that generates "meanders" to compensate

    for length differences, or to create a fixed total length of a

    differential pair.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

    Klaus Schmidinger wrote on Fri, 23 September 2011 03:46

    In V6 the (manual) ROUTE command will treat signals that have the

    same net class and the same name (one ending with '+' and the other

    with '-') as "differential pairs". When picking up one airwire of such

    a pair, both signals will be routed in parallel, keeping the distance

    as defined in the net class.

     

     

    It's good that you are adding the capbility to keep traces together, but

    this should not be driven from the net names.  Automatic features like that

    may seem like they are saving time, but in the long run always cause

    trouble.  If two signals are to be routed together, I want to tell Eagle

    that explicitly and never have it think it knows somehow on its own.  For

    example, I have some existing designs with signal names D+ and D-, but I

    don't necessarily want them routed together.

     

    Within the existing Eagle framework, it's probably best if this were a

    property of net classes.  When this property is set, then all signals in

    the class will be routed together.  It's up to me to explicitly put such

    signals in their own net class and then enable the property.  Please,

    nothing automatic.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kcadsoft
    0 kcadsoft over 14 years ago in reply to e14 Contributor

    On 09/26/11 14:02, Christian Bohrer wrote:

    "Klaus Schmidinger"<Klaus.Schmidinger@cadsoft.de>  a écrit dans le message de news:

    ...

    >> We mainly need the information which signals form a differential

    >> pair in the board - and there all we have is the name and net

    >> class.

     

    And why not an ATTRIBUTE for nets? Visible or not in schematic...

     

    ATTRIBUTEs are only available for parts/elements, not for

    nets/signals.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

     

    "Klaus Schmidinger" <Klaus.Schmidinger@cadsoft.de> a écrit dans le message de news:

    j5plqa$ve5$1@cheetah.cadsoft.de...

    On 09/26/11 12:06, Morten Leikvoll wrote:

    >> "Klaus Schmidinger"<Klaus.Schmidinger@cadsoft.de>  wrote in message

    >> news:j5ibr9$cn7$1@cheetah.cadsoft.de...

    >>

    >>> There has to be some way of identifying which two signals form

    >>> a differential pair, and that's going to be via the signal names.

    >>> We can discuss which way this is done, so if '+' and '-' appear

    >>> inappropriate, we could use "_P" and "_N".

    >>

    >> If the name matching is the best way, I suggest supporting these user

    >> parameters:

    >> -matchstring

    >> -match location (first,end,anywhere)

    >>

    >> or simply a single matchstring with room for wildcard in front or/and at

    >> tail.

    >>

    >> Examples:

    >> matchstring="(n/p)_*" for (n_clk,p_clk)

    >> matchstring="*(/-)" for (clk,clk-)

    >> matchstring="(+/-)" for (data0,data-0,data1,data-1,..,data+7,data-7)

    >> (ps:not using proper regexp here, just pseudo where * is a wildcard of

    >> unknown length)

     

    See my reply to Johann Glaser.

     

    >> I think support for these are needed, but I sense a high level of potential

    >> support cases. Maybe because you may want a mix of all these and can easily

    >> use wrong names.

    >> I would think a link to the complementary net would be much nicer. It could

    >> have been done with a new command so that ULP's can handle it in your

    >> preferred way.

    >> An alternative would be to handle a diff pair as a special 2 wire 'bus' at

    >> sch level, but I dont think the current bus implementation is suitable for

    >> that.

     

    We mainly need the information which signals form a differential

    pair in the board - and there all we have is the name and net

    class.

     

    And why not an ATTRIBUTE for nets? Visible or not in schematic...

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kcadsoft
    0 kcadsoft over 14 years ago in reply to e14 Contributor

    On 09/26/11 12:06, Morten Leikvoll wrote:

    "Klaus Schmidinger"<Klaus.Schmidinger@cadsoft.de>  wrote in message

    news:j5ibr9$cn7$1@cheetah.cadsoft.de...

     

    >> There has to be some way of identifying which two signals form

    >> a differential pair, and that's going to be via the signal names.

    >> We can discuss which way this is done, so if '+' and '-' appear

    >> inappropriate, we could use "_P" and "_N".

     

    If the name matching is the best way, I suggest supporting these user

    parameters:

    -matchstring

    -match location (first,end,anywhere)

     

    or simply a single matchstring with room for wildcard in front or/and at

    tail.

     

    Examples:

    matchstring="(n/p)_*" for (n_clk,p_clk)

    matchstring="*(/-)" for (clk,clk-)

    matchstring="(+/-)" for (data0,data-0,data1,data-1,..,data+7,data-7)

    (ps:not using proper regexp here, just pseudo where * is a wildcard of

    unknown length)

     

    See my reply to Johann Glaser.

     

    I think support for these are needed, but I sense a high level of potential

    support cases. Maybe because you may want a mix of all these and can easily

    use wrong names.

    I would think a link to the complementary net would be much nicer. It could

    have been done with a new command so that ULP's can handle it in your

    preferred way.

    An alternative would be to handle a diff pair as a special 2 wire 'bus' at

    sch level, but I dont think the current bus implementation is suitable for

    that.

     

    We mainly need the information which signals form a differential

    pair in the board - and there all we have is the name and net

    class.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

     

    "Klaus Schmidinger" <Klaus.Schmidinger@cadsoft.de> wrote in message

    news:j5ibr9$cn7$1@cheetah.cadsoft.de...

     

    There has to be some way of identifying which two signals form

    a differential pair, and that's going to be via the signal names.

    We can discuss which way this is done, so if '+' and '-' appear

    inappropriate, we could use "_P" and "_N".

     

    If the name matching is the best way, I suggest supporting these user

    parameters:

    -matchstring

    -match location (first,end,anywhere)

     

    or simply a single matchstring with room for wildcard in front or/and at

    tail.

     

    Examples:

    matchstring="(n/p)_*" for (n_clk,p_clk)

    matchstring="*(/-)" for (clk,clk-)

    matchstring="(+/-)" for (data0,data-0,data1,data-1,..,data+7,data-7)

    (ps:not using proper regexp here, just pseudo where * is a wildcard of

    unknown length)

     

    I think support for these are needed, but I sense a high level of potential

    support cases. Maybe because you may want a mix of all these and can easily

    use wrong names.

    I would think a link to the complementary net would be much nicer. It could

    have been done with a new command so that ULP's can handle it in your

    preferred way.

    An alternative would be to handle a diff pair as a special 2 wire 'bus' at

    sch level, but I dont think the current bus implementation is suitable for

    that.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 25.09.2011 14:07, schrieb James Morrison:

    Klaus Schmidinger wrote on Sat, 24 September 2011 05:04

    >>> And what about whole busses that should be routed together?

    >>

    >> The differential pair feature we are currently implementing is

    >> only about two signals being routed in parallel.

    >

    I think this is the crux of the debate here.  From what I've read (and

    posted), many of us are trying to extend this tool to match length across

    signals on a bus.  Also, there appears to be two tools that Klaus is

    discussing:  differential pair routing and automatic length matching.  As

    we haven't see the beta none of us outsiders have seen how this is

    implemented and how tightly the two tools are tied together.

     

    So I would say, that even though you aren't intending to allow length

    matching across a bus you should allow a way to specify signals in a diff

    pair that is scalable to an entire bus.  This way you could (and should)

    expand the function in the future.

     

    This way, it will also make sure they don't get implemented in such a way

    as it won't be extendable in the future.  The diff pair routing tool and

    the bus length matching tool should be independent tools, in my opinion.

     

    With these criteria in mind, I don't think identifying them via signal name

    makes sense.

     

    I would prefer to make this a bus property and say that diff pairs need to

    defined as their own bus.  You can unlimited number of busses (unlike net

    classes).  This also expands nicely to trace length matching across a bus.

    Maybe you have a bus flag called "differential" that you set to trigger the

    diff pair routing.

     

    Also note, I don't want the tool to just start routing things it thinks

    are differential.  I should have to explicitly tell it that the two signals

    are differential. This bus methodology above respects that.

     

    Cheers,

     

    James.

     

    Fully agreed James. Even if Klaus implements a diff-pair "only" now, it

    would benefit in future.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

    Klaus Schmidinger wrote on Sat, 24 September 2011 05:04

    And what about whole busses that should be routed together?

     

    The differential pair feature we are currently implementing is

    only about two signals being routed in parallel.

     

     

    I think this is the crux of the debate here.  From what I've read (and

    posted), many of us are trying to extend this tool to match length across

    signals on a bus.  Also, there appears to be two tools that Klaus is

    discussing:  differential pair routing and automatic length matching.  As

    we haven't see the beta none of us outsiders have seen how this is

    implemented and how tightly the two tools are tied together.

     

    So I would say, that even though you aren't intending to allow length

    matching across a bus you should allow a way to specify signals in a diff

    pair that is scalable to an entire bus.  This way you could (and should)

    expand the function in the future.

     

    This way, it will also make sure they don't get implemented in such a way

    as it won't be extendable in the future.  The diff pair routing tool and

    the bus length matching tool should be independent tools, in my opinion.

     

    With these criteria in mind, I don't think identifying them via signal name

    makes sense.

     

    I would prefer to make this a bus property and say that diff pairs need to

    defined as their own bus.  You can unlimited number of busses (unlike net

    classes).  This also expands nicely to trace length matching across a bus.

    Maybe you have a bus flag called "differential" that you set to trigger the

    diff pair routing.

     

    Also note, I don't want the tool to just start routing things it thinks

    are differential.  I should have to explicitly tell it that the two signals

    are differential. This bus methodology above respects that.

     

    Cheers,

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

    On 9/24/11 5:18 AM, Klaus Schmidinger wrote:

    I don't like this.

    The fact that two signals are paired has to be a property of these

    two signals, and the easiest and most straight forward way to

    do it is through their names, since each signal must have a way

    of knowing its "companion".

    >

    Klaus Schmidinger

     

    I don't like this because it reuses one feature for a different purpose.

    Think about how the 'static' keyword in the C/C++ programming languages

    has so many different uses (to mark functions, variables, class

    variables, etc.) It is confusing.

     

    This is my preferred interface:

     

    • In the Edit menu there is an item called "Differential Pairs"

    • The item presents a list of differential pairs, which have ARBITRARY

    names.

    • There is an ADD button which lets you select any two nets in the

    existing design (sorted by name) to be considered differential

    • There is an EDIT button which lets you set the property of this

    differential pair (spacing, line width, layer(s) that are allowed for

    routing, maximum trace length mismatch for DRC, etc.)

    • There is a DELETE button

     

    That's it. It has no relationship to net classes, it has no relationship

    to net names. It is simply one place on one menu that COMPLETELY

    configures differential pairs and does not rely on any implicit/implied

    things like names or net classes.

     

    Andrew.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

    Klaus Schmidinger wrote on Sat, 24 September 2011 05:04

    Net classes have a parameter that defines the minimum distance

    between either two of them, which results in a (triangular)

    matrix. That matrix would become rather bulky with a large

    number of net classes.

     

    I see, it's a squared problem.  I agree, net classes isn't how to define

    this then.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kcadsoft
    0 kcadsoft over 14 years ago in reply to e14 Contributor

    On 23.09.2011 21:27, Warren Brayshaw wrote:

    Klaus Schmidinger wrote:

     

    >>

    >> There has to be some way of identifying which two signals form

    >> a differential pair, and that's going to be via the signal names.

    >> We can discuss which way this is done, so if '+' and '-' appear

    >> inappropriate, we could use "_P" and "_N".

    >>

    >

    As the feature is only for manual routing I would favour a 'gather' command

    in which you specify the pair/pairs

    This could work a number of ways but something like an alias list. You would

    store the signal name pairs in this list and whenever you start to route a

    signal the list is consulted to determine if another signal must be routed.

    Using this method, signal names are irrelevant and negate the need for + -

    _P _N

     

    This list of pairings would need to be stored in the board file

     

    I don't like this.

    The fact that two signals are paired has to be a property of these

    two signals, and the easiest and most straight forward way to

    do it is through their names, since each signal must have a way

    of knowing its "companion".

     

    It would be the simplest method to just use a certain naming convention,

    like '+'/'-' or "_P"/"_N", but if you're afraid this might clash with

    existing projects, we could add a flag to each signal that makes it

    "part of a differential pair". However, this still would mean that the two

    signals forming the differential pair would have to follow a naming

    convention in order to be identified as a pair.

    I'd like to avoid this flag, though, because it makes things unnecessarily

    complex.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kcadsoft
    0 kcadsoft over 14 years ago in reply to e14 Contributor

    On 23.09.2011 21:27, Warren Brayshaw wrote:

    Klaus Schmidinger wrote:

     

    >>

    >> There has to be some way of identifying which two signals form

    >> a differential pair, and that's going to be via the signal names.

    >> We can discuss which way this is done, so if '+' and '-' appear

    >> inappropriate, we could use "_P" and "_N".

    >>

    >

    As the feature is only for manual routing I would favour a 'gather' command

    in which you specify the pair/pairs

    This could work a number of ways but something like an alias list. You would

    store the signal name pairs in this list and whenever you start to route a

    signal the list is consulted to determine if another signal must be routed.

    Using this method, signal names are irrelevant and negate the need for + -

    _P _N

     

    This list of pairings would need to be stored in the board file

     

    I don't like this.

    The fact that two signals are paired has to be a property of these

    two signals, and the easiest and most straight forward way to

    do it is through their names, since each signal must have a way

    of knowing its "companion".

     

    It would be the simplest method to just use a certain naming convention,

    like '+'/'-' or "_P"/"_N", but if you're afraid this might clash with

    existing projects, we could add a flag to each signal that makes it

    "part of a differential pair". However, this still would mean that the two

    signals forming the differential pair would have to follow a naming

    convention in order to be identified as a pair.

    I'd like to avoid this flag, though, because it makes things unnecessarily

    complex.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

    On 9/24/11 5:18 AM, Klaus Schmidinger wrote:

    I don't like this.

    The fact that two signals are paired has to be a property of these

    two signals, and the easiest and most straight forward way to

    do it is through their names, since each signal must have a way

    of knowing its "companion".

    >

    Klaus Schmidinger

     

    I don't like this because it reuses one feature for a different purpose.

    Think about how the 'static' keyword in the C/C++ programming languages

    has so many different uses (to mark functions, variables, class

    variables, etc.) It is confusing.

     

    This is my preferred interface:

     

    • In the Edit menu there is an item called "Differential Pairs"

    • The item presents a list of differential pairs, which have ARBITRARY

    names.

    • There is an ADD button which lets you select any two nets in the

    existing design (sorted by name) to be considered differential

    • There is an EDIT button which lets you set the property of this

    differential pair (spacing, line width, layer(s) that are allowed for

    routing, maximum trace length mismatch for DRC, etc.)

    • There is a DELETE button

     

    That's it. It has no relationship to net classes, it has no relationship

    to net names. It is simply one place on one menu that COMPLETELY

    configures differential pairs and does not rely on any implicit/implied

    things like names or net classes.

     

    Andrew.