Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) USB routing problems : D+/- length issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 30 replies
  • Answers 2 answers
  • Subscribers 191 subscribers
  • Views 3518 views
  • Users 0 members are here
  • length
  • d-
  • autorouter
  • usb
  • parallelism
  • d+
Related

USB routing problems : D+/- length issues

e14 Contributor
e14 Contributor over 14 years ago

Hello everyone

 

I'm a user of Eagle for 2 years now, and i'm trying to make USB with an Overo and a dsPIC.

The thing is that I had read somewhere (http://www.usb.org/developers/docs/hs_usb_pdg_r1_0.pdf) that the signals D+ and D- must have the same length (they talk about non parallelism page 10 figure 5)

 

But here is the point : how you do that on Eagle , to force 2 wire to have the same length (or being parallel all the way), in autorouter mode of course but even in manual mode.

 

Thanks for the help .

 

Best Regards

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Vincent Vittori schrieb:

     

    I'm a user of Eagle for 2 years now, and i'm trying to make USB with

    an Overo and a dsPIC. The thing is that I had read somewhere

    (http://www.usb.org/developers/docs/hs_usb_pdg_r1_0.pdf) that the

    signals D+ and D- must have the same length (they talk about non

    parallelism page 10 figure 5)

     

    But here is the point : how you do that on Eagle , to force 2 wire to

    have the same length (or being parallel all the way), in autorouter

    mode of course but even in manual mode.

     

    First of all, I would never use the autorouter for this. (I don't use it

    at all... but here it's essential.)

     

    Then, simply (manually) route your tracks as parallel as possible. You

    can check their length with an ULP and correct them if necessary.

     

    In EAGLE, there is no way to /force/ an equally long differential pair

    during routing, neither manually nor by autorouter. Maybe V6 will add

    something new here, but I don't know.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kcadsoft
    0 kcadsoft over 14 years ago in reply to e14 Contributor

    On 09/23/11 08:08, Tilmann Reh wrote:

    ...

    In EAGLE, there is no way to /force/ an equally long differential pair

    during routing, neither manually nor by autorouter. Maybe V6 will add

    something new here, but I don't know.

     

    In V6 the (manual) ROUTE command will treat signals that have the

    same net class and the same name (one ending with '+' and the other

    with '-') as "differential pairs". When picking up one airwire of such

    a pair, both signals will be routed in parallel, keeping the distance

    as defined in the net class.

     

    This can't guarantee the same length for both signals, so there

    will also be a new command that generates "meanders" to compensate

    for length differences, or to create a fixed total length of a

    differential pair.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kcadsoft

    "Klaus Schmidinger" <Klaus.Schmidinger@cadsoft.de> wrote in message

    news:j5hdh5$va6$1@cheetah.cadsoft.de...

    In V6 the (manual) ROUTE command will treat signals that have the

    same net class and the same name (one ending with '+' and the other

    with '-') as "differential pairs". When picking up one airwire of such

    a pair, both signals will be routed in parallel, keeping the distance

    as defined in the net class.

     

    You should be a bit careful about using the + and - signs. It works as long

    as you dont export netfiles to other tools, but + and - in names are often a

    source of confusion and problems. As an example, we export netnames

    connected to FPGA's and feed them into the pin assignment files. That tool

    will not allow + and - and simply replacing it with something else is a

    potential source of conflict.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kcadsoft
    0 kcadsoft over 14 years ago in reply to Johann.Glaser@gmx.at

    On 09/24/11 11:46, Johann Glaser wrote:

    Hi!

     

    Am Freitag, den 23.09.2011, 18:24 +0200 schrieb Klaus Schmidinger:

    >> On 23.09.2011 15:47, Morten Leikvoll wrote:

    >>> "Klaus Schmidinger"<Klaus.Schmidinger@cadsoft.de>   wrote in message

    >>> news:j5hdh5$va6$1@cheetah.cadsoft.de...

    >>>> In V6 the (manual) ROUTE command will treat signals that have the

    >>>> same net class and the same name (one ending with '+' and the other

    >>>> with '-') as "differential pairs". When picking up one airwire of such

    >>>> a pair, both signals will be routed in parallel, keeping the distance

    >>>> as defined in the net class.

    >>>

    >>> You should be a bit careful about using the + and - signs. It works as long

    >>> as you dont export netfiles to other tools, but + and - in names are often a

    >>> source of confusion and problems. As an example, we export netnames

    >>> connected to FPGA's and feed them into the pin assignment files. That tool

    >>> will not allow + and - and simply replacing it with something else is a

    >>> potential source of conflict.

    >>

    >> We could just as well use something more exotic, like "_P" and "_N".

     

    I second the thoughts on the '+' and '-' chars in names.

     

    As you have written, you don't like to add another kind of a setting to

    specify which signals belong together, we might only have the naming.

     

    What do you think of making the naming configurable? The default could

    be:

      - '-' / '+'

      - '_n' / '_p'

    (both, but only within its little groups). But this should be possible

    to change with a dialog or "set" command. If somebody wants signals with

    that name ending, but not have them routed together, just remove the

    setting for that schematic/board. If somebody wants special name endings

    for differential pairs, e.g. '_PLUS' and '_MINUS', he simply sets it

    accordingly.

     

    So it would be nice to have zero to "a few" pair name ends to be setup.

     

    This would mean the selection would have to be stored in the schematic/board,

    and thus would make combining two files from different sources

    ("design reuse") virtually impossibe.

     

    A fixed convention avoids such problems altogether.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Johann.Glaser@gmx.at

    Johann Glaser <Johann.Glaser@gmx.at> wrote:

    Hi!

     

    Am Freitag, den 23.09.2011, 18:24 +0200 schrieb Klaus Schmidinger:

    >> On 23.09.2011 15:47, Morten Leikvoll wrote:

    >>> "Klaus Schmidinger"<Klaus.Schmidinger@cadsoft.de>  wrote in message

    >>> news:j5hdh5$va6$1@cheetah.cadsoft.de...

    >>>> In V6 the (manual) ROUTE command will treat signals that have the

    >>>> same net class and the same name (one ending with '+' and the other

    >>>> with '-') as "differential pairs". When picking up one airwire of such

    >>>> a pair, both signals will be routed in parallel, keeping the distance

    >>>> as defined in the net class.

    >>>

    >>> You should be a bit careful about using the + and - signs. It works as long

    >>> as you dont export netfiles to other tools, but + and - in names are often a

    >>> source of confusion and problems. As an example, we export netnames

    >>> connected to FPGA's and feed them into the pin assignment files. That tool

    >>> will not allow + and - and simply replacing it with something else is a

    >>> potential source of conflict.

    >>

    >> We could just as well use something more exotic, like "_P" and "_N".

     

    I second the thoughts on the '+' and '-' chars in names.

     

    As you have written, you don't like to add another kind of a setting to

    specify which signals belong together, we might only have the naming.

     

    What do you think of making the naming configurable? The default could

    be:

    - '-' / '+'

    - '_n' / '_p'

    (both, but only within its little groups). But this should be possible

    to change with a dialog or "set" command. If somebody wants signals with

    that name ending, but not have them routed together, just remove the

    setting for that schematic/board. If somebody wants special name endings

    for differential pairs, e.g. '_PLUS' and '_MINUS', he simply sets it

    accordingly.

     

    So it would be nice to have zero to "a few" pair name ends to be setup.

     

    You also have to consider that its not always practical to have this in the

    suffix. A prefix is just as logical. Also somewhere in the middle. Think

    for example an lvds BUS where you want an numeric index as prefix.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • KE5FX
    0 KE5FX over 14 years ago in reply to Johann.Glaser@gmx.at

    Would it be reasonable to make this a bus property, rather than a property of net classes or of individual signals?  As long as you allow nets to be part of more than one logical bus, it's not a big hardship to require users to associate a bus with signals that need to be routed for minimal timing skew.

     

    Using bus notation would permit groups of more than two signals to be routed for equal length, which IMHO is required for this feature to be of any real use.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • KE5FX
    0 KE5FX over 14 years ago in reply to Johann.Glaser@gmx.at

    Would it be reasonable to make this a bus property, rather than a property of net classes or of individual signals?  As long as you allow nets to be part of more than one logical bus, it's not a big hardship to require users to associate a bus with signals that need to be routed for minimal timing skew.

     

    Using bus notation would permit groups of more than two signals to be routed for equal length, which IMHO is required for this feature to be of any real use.