Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Change wire cap
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 2031 views
  • Users 0 members are here
Related

Change wire cap

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I have been having a play around with the layout editor in eagle to familiarize myself with the basics of PCB design. However, I have ran into what should be quite a simple problem.

 

I need the end of the wire to be flat instead of rounded, because with the rounded end the trace 'spills' over the other side of the pad with the trace thickness that I want, since the pad is relatively thin. If the end were flat, then this would not happen. There is the option in the properties dialog with the cap set to round, but this is grayed out and cannot be changed. The change tool won't change the cap to flat either.

 

Any advice? It seems like the problem should be simple to fix but I can't see any obvious options.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 09/29/2011 08:05 AM, Kieran Martin wrote:

    Hi,

     

    I have been having a play around with the layout editor in eagle to familiarize myself with the basics of PCB design. However, I have ran into what should be quite a simple problem.

     

    I need the end of the wire to be flat instead of rounded, because with the rounded end the trace 'spills' over the other side of the pad with the trace thickness that I want, since the pad is relatively thin. If the end were flat, then this would not happen. There is the option in the properties dialog with the cap set to round, but this is grayed out and cannot be changed. The change tool won't change the cap to flat either.

     

    Any advice? It seems like the problem should be simple to fix but I can't see any obvious options.

     

    One other option to power supply traces that need to vary is size it to

    use polygons for them. It is a little more work to start with using the

    polygon properties get the maximum thickness that passes DRC.

     

    Paul R.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks for the response Paul.

     

    Do you know if it is possible to use pollygons with the follow-me method? I've been using the forward/back or follow-me method to ensure that everything is hooked up correctly with regards to the schematic.

     

    The problem seems very odd to me, since if you go into the properties of the wire and add a curve, you suddenly get the option to make the end of the wire flat. But once you return to having no curve on the wire, the option is greyed out and forced to rounded end.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks for the response Paul.

     

    Do you know if it is possible to use pollygons with the follow-me method? I've been using the forward/back or follow-me method to ensure that everything is hooked up correctly with regards to the schematic.

     

    The problem seems very odd to me, since if you go into the properties of the wire and add a curve, you suddenly get the option to make the end of the wire flat. But once you return to having no curve on the wire, the option is greyed out and forced to rounded end.