EAGLE User Support (English) EAGLEDIR
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
  • Replies 5 replies
  • Subscribers 178 subscribers
  • Views 995 views
  • Users 0 members are here
Related

EAGLEDIR

Phil_Keller
Phil_Keller over 17 years ago

I have just upgraded to Eagle 5.0 and then upgraded to 5.1.  I have a

Non-profit Standard License.  When I start the 5.x program the library

is pointed to by the variable $EAGLEDIR that is currently set to my 4.16

libraries.  I am not ready to remove 4.16 as some of the designs are

still there and I have not yet made the transition fully to 5.

 

   Where is the value of EAGLEDIR set and how can I change it to point

to the 5.0 structure?

 

   Thanks,

Phil

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Phil wrote:

    Klaus,

     

      Well kind-of.  What I think I understand is the following.

     

      For some reason the "Library Use" list included all the libraries in

    the 4.16 structure.

     

      When I look at the libraries in the Library list in the Control

    Panel I see the libraries in 5.1.  If I open a schematic that was

    created in 5.1 and click "add" the libraries are in the 4.16 structure (as

    shown

    by the path displayed and their contents).  Dropping them and then

    adding the 5.1 libraries seems to have solve the problem.

     

    I have experienced the same thing more than once when upgrading to a new

    version of Eagle.  And yet when I type "open somelib" in the schematic

    editor, it opens a library in the new Eagle directory.  That becomes very

    confusing when you create a new device in a library, then go to Add it to

    your schematic, and it's not there!  I also have solved the problem by

    dropping all libs and adding the correct ones.

     

    --

    Bert Menkveld

     

     

      It still seems strange to me that it pointed to the 4.16 but a

    solution is at hand.

     

      Danke,

    Phil

     

    Klaus Schmidinger wrote:

    On 07/22/08 05:06, Phil wrote:

     

    I have just upgraded to Eagle 5.0 and then upgraded to 5.1.  I have

    a Non-profit Standard License.  When I start the 5.x program the

    library is pointed to by the variable $EAGLEDIR that is currently

    set to my 4.16 libraries.  I am not ready to remove 4.16 as some of the

    designs are still there and I have not yet made the transition

    fully to 5. Where is the value of EAGLEDIR set and how can I change it

    to

    point to the 5.0 structure?

     

    EAGLEDIR ist the directory that contains the version of EAGLE

    you are currently running.

    It is determined at runtime, by taking the full path name to

    the eagle.exe file and stripping the "\bin\eagle.exe" part.

     

    So if you have installed EAGLE into

     

      C:\Program files\EAGLE-5.1.0

     

    the EAGLEDIR variable will contain the value "C:\Program

    files\EAGLE-5.1.0".

    when you run "C:\Program files\EAGLE-5.1.0\bin\eagle.exe".

     

    Klaus Schmidinger

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Phil wrote:

    Klaus,

     

      Well kind-of.  What I think I understand is the following.

     

      For some reason the "Library Use" list included all the libraries in

    the 4.16 structure.

     

      When I look at the libraries in the Library list in the Control

    Panel I see the libraries in 5.1.  If I open a schematic that was

    created in 5.1 and click "add" the libraries are in the 4.16 structure (as

    shown

    by the path displayed and their contents).  Dropping them and then

    adding the 5.1 libraries seems to have solve the problem.

     

    I have experienced the same thing more than once when upgrading to a new

    version of Eagle.  And yet when I type "open somelib" in the schematic

    editor, it opens a library in the new Eagle directory.  That becomes very

    confusing when you create a new device in a library, then go to Add it to

    your schematic, and it's not there!  I also have solved the problem by

    dropping all libs and adding the correct ones.

     

    --

    Bert Menkveld

     

     

      It still seems strange to me that it pointed to the 4.16 but a

    solution is at hand.

     

      Danke,

    Phil

     

    Klaus Schmidinger wrote:

    On 07/22/08 05:06, Phil wrote:

     

    I have just upgraded to Eagle 5.0 and then upgraded to 5.1.  I have

    a Non-profit Standard License.  When I start the 5.x program the

    library is pointed to by the variable $EAGLEDIR that is currently

    set to my 4.16 libraries.  I am not ready to remove 4.16 as some of the

    designs are still there and I have not yet made the transition

    fully to 5. Where is the value of EAGLEDIR set and how can I change it

    to

    point to the 5.0 structure?

     

    EAGLEDIR ist the directory that contains the version of EAGLE

    you are currently running.

    It is determined at runtime, by taking the full path name to

    the eagle.exe file and stripping the "\bin\eagle.exe" part.

     

    So if you have installed EAGLE into

     

      C:\Program files\EAGLE-5.1.0

     

    the EAGLEDIR variable will contain the value "C:\Program

    files\EAGLE-5.1.0".

    when you run "C:\Program files\EAGLE-5.1.0\bin\eagle.exe".

     

    Klaus Schmidinger