Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) changing thermal PADs for LED's
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 189 subscribers
  • Views 590 views
  • Users 0 members are here
  • pour
Related

changing thermal PADs for LED's

mike111
mike111 over 14 years ago

I'm designing an aluminium single layer board with multiple high power LED's. I use an aluminium board for cooling these powerful LED's. I want to make the thermal PAD for the LED's bigger than the PAD in the library. Because I use quite a large number lot of LED's and the surrounding of each LED is different I cannot change the library model, but have to change each PAD individually. But because the thermal PADs are not electrically isolated I cannot make a ground plane to put them on as I did with other types. Is there a trick to easily pour some copper on these pads? Or is there another solution to make the PADs bigger in Eagle light?

Thanks!

  • Sign in to reply
  • Cancel
  • mike111
    0 mike111 over 14 years ago in reply to e14 Contributor

    thanks! helped a lot

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to mike111

    mike111 schrieb:

     

    Thanks for the reply. I'm using Ledengin LZ1's. But I can't find the

    net name of the thermal contact. It seems there is no net name for

    that. how can I change that?

     

    In the schematic, draw a short net stub at the related pin and name it

    somehow. Use the same name for the polygon in the board.

     

    (If there is no pin in the schematic, correct the device in the library.)

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mike111
    0 mike111 over 14 years ago in reply to e14 Contributor

    Thanks for the reply. I'm using Ledengin LZ1's. But I can't find the net name of the thermal contact. It seems there is no net name for that. how can I change that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 10/12/2011 06:23 AM, mike111 wrote:

    I'm designing an aluminium single layer board with multiple high power LED's. I use an aluminium board for cooling these powerful LED's. I want to make the thermal PAD for the LED's bigger than the PAD in the library. Because I use quite a large number lot of LED's and the surrounding of each LED is different I cannot change the library model, but have to change each PAD individually. But because the thermal PADs are not electrically isolated I cannot make a ground plane to put them on as I did with other types. Is there a trick to easily pour some copper on these pads? Or is there another solution to make the PADs bigger in Eagle light?

    Thanks!

     

    Use a small polygon around the pad and name it the net name of the pad.

    You can turn thermals off on that polygon. You may also need to use rank

    for overlapping cases. See help rank.