Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) A disgusted problem —— the keyboard is often locked by EAGLE
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 188 subscribers
  • Views 746 views
  • Users 0 members are here
  • eagle
Related

A disgusted problem —— the keyboard is often locked by EAGLE

e14 Contributor
e14 Contributor over 14 years ago

Hi everyone

 

Several weeks ago, I changed the OS from Win7 to  Fedora. Fortunately, the EAGLE can be used under Fedora and its UI is highly similar to what it is in Win7. But when I began to work with it, a problem occurred. After I added a component into a scheme, and then canceled the adding by pressing ESC, as same as I usually did in Win7, the keyboard was locked. That means, I couldn't type anything and even couldn't close a dialogbox by pressing ESC anymore. I didn't know what happened at the time. So I planed to close the EAGLE. But to my surprise, when I tried to save  the scheme, I couldn't type filename. Another words, the keyboard was completely locked. I forced to close the EAGLE then opened it again. All were OK. But latter, due to some unknown reasons, the problem occurred again and again. I realized that it's not a accident. So I googled it but couldn't get any valuable information. Has anybody here ever met this problem? Is anybody here can give some advice to solve it?

 

Best regards.

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    0 Richard_H over 14 years ago

    Am 25.10.2011 08:41, schrieb Rui Ma:

    Hi everyone

     

    Several weeks ago, I changed the OS from Win7 to  Fedora. Fortunately, the EAGLE can be used under Fedora and its UI is highly similar to what it is in Win7. But when I began to work with it, a problem occurred. After I added a component into a scheme, and then canceled the adding by pressing ESC, as same as I usually did in Win7, the keyboard was locked. That means, I couldn't type anything and even couldn't close a dialogbox by pressing ESC anymore. I didn't know what happened at the time. So I planed to close the EAGLE. But to my surprise, when I tried to save  the scheme, I couldn't type filename. Another words, the keyboard was completely locked. I forced to close the EAGLE then opened it again. All were OK. But latter, due to some unknown reasons, the problem occurred again and again. I realized that it's not a accident. So I googled it but couldn't get any valuable information. Has anybody here ever met this problem? Is anybody here can give some advice to solve it?

     

     

    Best regards.

     

     

    You write the keyboard was locked, but you could move/use the mouse.

    Could you type something for example in a terminal window or in

    another application in this situation?

     

    What when you are pressing escape in another situation in EAGLE,

    let's say with the ROUTE command acive? Is the keyboard locked as

    well then?

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Richard_H

    Yes, the keyboard is OK in another applications for example a terminal window. With the ROUTE command avtive, and when I press ESC, it will quit ROUTE mode immediately. The keyboard will not be locked under this situation. It seems that the problem only occurs in schematic mode.

     

    Let me describe the problem step by step again:

     

    1) Opened EAGLE.

     

    2) Created a new project.

     

    3) Created a new schematic in the project.

     

    4) Tried to add a componet. A componet category dialogbox appeared.

     

    5) Here I want to add a resistor. So I selected the certain component. A R1 appeared in schematic. And, after that, the software was still in adding mode. I could see an other resistor which color is red floated above the schmatic. Of course I could directly add it by just clicking mouse. But I didn't want to add resistors anymore. So I pressed ESC. The category dialogbox appeared again. I pressed ESC again. Another words, I continuely pressed ESC twice. OK, that problem occured!

     

    P.S. The OS I am using is Fedora15 and the language is Simplefied Chinese.

     

    Best regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 14 years ago in reply to e14 Contributor

    Am 26.10.2011 09:10, schrieb Rui Ma:

    Yes, the keyboard was OK in another aapplications for example a

    terminate. With the ROUTE command avtive, and whennever I press ESC,

    it will quit ROUTE mode immediately and the keyboard will not be

    locked under this situation. It seems that the problem only occures

    when editing scheme.

     

    Let me describe the problem step by step again:

     

    1) Opened EAGLE.

     

    2) Created a new project.

     

    3) Created a new schematic in the project.

     

    4) Tried to add a componet. A componet category dialogbox appeared.

     

    5) Here I want to add a resistor. So I selected the certain

    component. A R1 appeared in schematic. And, after that, the software

    was still in adding mode. I could see an other resistor which color

    is red floated above the schmatic. Of course I could directly add it

    by just clicking mouse. But I didn't want to add resistors anymore.

    So I pressed ESC. A dialogbox appeared. But I didn't want to add any

    componets either. So I pressed ESC again. Another words, I continuely

    pressed ESC twice. OK, that problem occured!

     

    P.S. The OS I am using is Fedora15 and the language is Simplefied

    Chinese.

     

    Best regards

     

     

     

    Could you please check whether it is possible to lock the keyboard

    by presing Esc key twice or more times in any other situation in EAGLE?

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Rui Ma Inscribed thus:

     

    Yes. It's probably a kind of "race" issue, but I don't think it's

    about Fedora, I guess it's about GNOME. Because I tried it on an toher

    computer which setup Linuxmint11, the problem occured once time. They

    are all use GNOME. About OpenSUSE, I'm not sure, I never used it. But

    I heard that it's based on KDE. Later I'll try.

     

    Thanks for Baron.

     

    Yes I use the KDE 3.5.10 desktop on Open SuSE 11.1.

    I find KDE 4 almost unusable in comparison.  Why on earth they decided

    to alienate users by doing a wholesale dump and re-write, rather than a

    phased introduction...

     

    I belive that Open SuSE is going to prefer Gnome to KDE in the next

    release.  I'll not hold my breath...

     

    --

    Best Regards:

                         Baron.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Yes. It's probably a kind of "race" issue, but I don't think it's about Fedora, I guess it's about GNOME. Because I tried it on an oher computer which runs Linuxmint11, the problem occured once time again. They are all use GNOME. For OpenSUSE, I'm not sure, I never used it. But I heard that it's based on KDE. Later I'll try.

     

    Thanks for Baron.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Rui Ma Inscribed thus:

     

    I had a new find! The problem only occurs when I try to clean the

    adding components dialogbox too quickly. What I mean is, when I

    succeed adding a componet into schematic and needn't more adding, I

    usually cancel the execution by pressing ESC twice. After the 1st

    pressing, the dialogbox appears, as I do want to exit, the 2nd

    pressing will be performed without stop. After that, the keyboard is

    locked. If I stop a moment between the twice pressing, for example

    wait one second, nothing happens.

     

    And, I did a varity of test as per Hammerl's advice. It seems that

    only adding components can cause the problem.

     

    Best Regards

     

    I followed Rui's directions and couldn't reproduce the problem (Open

    SuSE 11.1), Eagle 5.10...

    It does sound like some kind of "race" issue in Fedora.

     

    HTH.

     

    --

    Best Regards:

                         Baron.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Richard_H

    I had a new find! The problem only occurs when I try to clean the adding components dialogbox too quickly. What I mean is, when I succeed adding a componet into schematic and needn't more adding, I usually cancel the execution by pressing ESC twice. After the 1st pressing, the dialogbox appears, as I do want to exit, the 2nd pressing will be performed without stopping. After that, the keyboard is locked. If I stop a moment between the twice pressing, for example wait about one second, all will be OK.

     

    And, I did a varity of tests as per Hammerl's advice. It seems that only adding components can cause the problem.

     

    Best Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Richard_H

    I had a new find! The problem only occurs when I try to clean the adding components dialogbox too quickly. What I mean is, when I succeed adding a componet into schematic and needn't more adding, I usually cancel the execution by pressing ESC twice. After the 1st pressing, the dialogbox appears, as I do want to exit, the 2nd pressing will be performed without stopping. After that, the keyboard is locked. If I stop a moment between the twice pressing, for example wait about one second, all will be OK.

     

    And, I did a varity of tests as per Hammerl's advice. It seems that only adding components can cause the problem.

     

    Best Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Rui Ma Inscribed thus:

     

    Yes. It's probably a kind of "race" issue, but I don't think it's

    about Fedora, I guess it's about GNOME. Because I tried it on an toher

    computer which setup Linuxmint11, the problem occured once time. They

    are all use GNOME. About OpenSUSE, I'm not sure, I never used it. But

    I heard that it's based on KDE. Later I'll try.

     

    Thanks for Baron.

     

    Yes I use the KDE 3.5.10 desktop on Open SuSE 11.1.

    I find KDE 4 almost unusable in comparison.  Why on earth they decided

    to alienate users by doing a wholesale dump and re-write, rather than a

    phased introduction...

     

    I belive that Open SuSE is going to prefer Gnome to KDE in the next

    release.  I'll not hold my breath...

     

    --

    Best Regards:

                         Baron.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Yes. It's probably a kind of "race" issue, but I don't think it's about Fedora, I guess it's about GNOME. Because I tried it on an oher computer which runs Linuxmint11, the problem occured once time again. They are all use GNOME. For OpenSUSE, I'm not sure, I never used it. But I heard that it's based on KDE. Later I'll try.

     

    Thanks for Baron.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Rui Ma Inscribed thus:

     

    I had a new find! The problem only occurs when I try to clean the

    adding components dialogbox too quickly. What I mean is, when I

    succeed adding a componet into schematic and needn't more adding, I

    usually cancel the execution by pressing ESC twice. After the 1st

    pressing, the dialogbox appears, as I do want to exit, the 2nd

    pressing will be performed without stop. After that, the keyboard is

    locked. If I stop a moment between the twice pressing, for example

    wait one second, nothing happens.

     

    And, I did a varity of test as per Hammerl's advice. It seems that

    only adding components can cause the problem.

     

    Best Regards

     

    I followed Rui's directions and couldn't reproduce the problem (Open

    SuSE 11.1), Eagle 5.10...

    It does sound like some kind of "race" issue in Fedora.

     

    HTH.

     

    --

    Best Regards:

                         Baron.