Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) "Via in Pad" not allowed? Tell me it ain't so!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 190 subscribers
  • Views 2356 views
  • Users 0 members are here
Related

"Via in Pad" not allowed? Tell me it ain't so!

MontanaEE
MontanaEE over 14 years ago

Okay, I have a very tight layout.  Real estate on the board is premium.  I need to be able to run quite a few vias directly into a "same signal" pad on an SMD component.

 

Distance in DR's is set to 0 for same signal.

 

Board is set up to do this, but when I route to one of these points and try to place a via, I get the "big yellow X" instead.  I do not have blind and buried vias enabled (MicroVia set to 9.99mm) and this is a 6 layer board (1+2*3+14*15+16).  Via should go from layer 1 to 16, and works fine unless I try to put it at an SMD pad.

 

How do I get the editor to allow a Via In Pad?

 

Gone through the manual again..check.

Browsed the forums and found one where someone was asking about Via in Pad for BGA's, but when I try that solution, DRC has a conniption fit, and then I have one.......

 

Stephen

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 14 years ago

    On 12/11/2011 01:32 AM, Stephen Doll wrote:

    Okay, I have a very tight layout.  Real estate on the board is

    premium.  I need to be able to run quite a few vias directly into a

    "same signal" pad on an SMD component.

     

    Distance in DR's is set to 0 for same signal.

     

    Board is set up to do this, but when I route to one of these points

    and try to place a via, I get the "big yellow X" instead.

     

    The yellow X tells you that the via is placed at the end of a route but

    is not logically connected.  This also appears when routes on different

    layers end at the same point.

     

    After you place the via do a ratsnest.

     

    HTH,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dukepro
    0 dukepro over 14 years ago

    On 12/11/2011 01:32 AM, Stephen Doll wrote:

    Okay, I have a very tight layout.  Real estate on the board is

    premium.  I need to be able to run quite a few vias directly into a

    "same signal" pad on an SMD component.

     

    Distance in DR's is set to 0 for same signal.

     

    Board is set up to do this, but when I route to one of these points

    and try to place a via, I get the "big yellow X" instead.

     

    The yellow X tells you that the via is placed at the end of a route but

    is not logically connected.  This also appears when routes on different

    layers end at the same point.

     

    After you place the via do a ratsnest.

     

    HTH,

        - Chuck