Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Via without effect (wirkungslos) if Drill > 0 [ref. to design rules/masks/limit]
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 189 subscribers
  • Views 342 views
  • Users 0 members are here
  • board
  • eagle
  • question
Related

Via without effect (wirkungslos) if Drill > 0 [ref. to design rules/masks/limit]

Wolfskammer04
Wolfskammer04 over 14 years ago

How can I avoid and remedy this 'Drill Size' error?

and btw I am very careful to put only one via to the board, but often when want to move it later on I find that it consists of two parts (or two vias). Is there anything I am doing wrong here?

 

Roland

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Wolfskammer04 <noreply-37378@element14.com> wrote:

    How can I avoid and remedy this 'Drill Size' error?

    and btw I am very careful to put only one via to the board, but often

    when want to move it later on I find that it consists of two parts (or

    two vias). Is there anything I am doing wrong here?

     

    Roland

     

    You are probably not aware that the via is addred automatically when you

    route and change layer during routing?

    Another option could be an uncontrolled copy action.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Wolfskammer04
    0 Wolfskammer04 over 14 years ago in reply to e14 Contributor

    That is not really the case. I am very careful when I add vias. So by all means a via has to consist of only one element - Right?

    How shouold I solve this ' without effect' error correctly. Replace it by a new one?

    Roland

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Wolfskammer04
    0 Wolfskammer04 over 14 years ago in reply to Wolfskammer04

    I found the solution myself. The reason for that 'Drill Size' error is caused by different measurement units for the real drill size in mm (here 0.6) and the settings for it's limits (here 24mil). But 24 mil equal 0.6096 mm so 0.6 is too small. I changed it directly in the board file using notepad++'s replace function.

    ...and all worked fine.

     

    Roland

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Wolfskammer04
    0 Wolfskammer04 over 14 years ago in reply to Wolfskammer04

    I found the solution myself. The reason for that 'Drill Size' error is caused by different measurement units for the real drill size in mm (here 0.6) and the settings for it's limits (here 24mil). But 24 mil equal 0.6096 mm so 0.6 is too small. I changed it directly in the board file using notepad++'s replace function.

    ...and all worked fine.

     

    Roland