Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Additional import and export features
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 916 views
  • Users 0 members are here
  • cad
  • features
Related

Additional import and export features

e14 Contributor
e14 Contributor over 14 years ago

I badly need 2 items.

 

1.  An import function into librarys that can provide the mechanical structure for components.  Ideally, something like a DXF.importer into the

dimension layer.  Components that have mechanical features in addition to the basic part connection pads need a lot of effort to create.  This

is usually a duplicate effort from a mechanical design done outside of Eagle.

 

2. An export function other than pixels out of the board layout.  Again, ideally DXF.  This would allow more precice integration of the finished

board into exernal CAD programs (That board has to go live someplace after it is done).  Currently I have to do a hack and plot out into HPGL,

then convert it to DXF.  This is imprecise and requires clean-up of the DXF to get critical dimensions correct.

 

Any recommendations?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 26.01.2012 01:32, Joe Mickley wrote:

      I badly need 2 items.

     

    1.  An import function into librarys that can provide the mechanical structure for components.  Ideally, something like a DXF.importer into the

    dimension layer.  Components that have mechanical features in addition to the basic part connection pads need a lot of effort to create.  This

    is usually a duplicate effort from a mechanical design done outside of Eagle.

     

     

    There are some tools that allow conversion from DXF to EAGLE script.

    ==> http://www.cadsoft.de/downloads/tools-and-converters

     

    for example

      dxf2scr-1.zip  (for free)

      eagle_pcb_power_tools*.exe

     

     

     

    2. An export function other than pixels out of the board layout.  Again, ideally DXF.  This would allow more precice integration of the finished

    board into exernal CAD programs (That board has to go live someplace after it is done).  Currently I have to do a hack and plot out into HPGL,

    then convert it to DXF.  This is imprecise and requires clean-up of the DXF to get critical dimensions correct.

     

    Any recommendations?

     

     

    Use DXF.ULP.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 26.01.2012 01:32, Joe Mickley wrote:

      I badly need 2 items.

     

    1.  An import function into librarys that can provide the mechanical structure for components.  Ideally, something like a DXF.importer into the

    dimension layer.  Components that have mechanical features in addition to the basic part connection pads need a lot of effort to create.  This

    is usually a duplicate effort from a mechanical design done outside of Eagle.

     

     

    There are some tools that allow conversion from DXF to EAGLE script.

    ==> http://www.cadsoft.de/downloads/tools-and-converters

     

    for example

      dxf2scr-1.zip  (for free)

      eagle_pcb_power_tools*.exe

     

     

     

    2. An export function other than pixels out of the board layout.  Again, ideally DXF.  This would allow more precice integration of the finished

    board into exernal CAD programs (That board has to go live someplace after it is done).  Currently I have to do a hack and plot out into HPGL,

    then convert it to DXF.  This is imprecise and requires clean-up of the DXF to get critical dimensions correct.

     

    Any recommendations?

     

     

    Use DXF.ULP.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 26.01.2012 16:33, schrieb Richard Hammerl:

    Use DXF.ULP.

     

    The question about DXF output has been asked twelve billion times, and a

    lot of users surely don't know that EAGLE can do a thing like that. And

    why is that so? Because the DXF output is NOT available via the GUI.

    Every user searches for a function like that

      - in the 'save' or 'save as' dialogs and

      - in the 'export' function (that's where it belongs).

    DXF is nowhere mentioned -> Conclusion: EAGLE cannot do that.

     

    For the DXF import, I can understand that CadSoft doesn't want to

    program this, since it's quite some work. But for the DXF output: This

    already HAS been programmed, so why not put it into the program proper

    and make it available with the EXPORT command? Doing things with

    external ULPs is something that the typical user doesn't want to fiddle

    around with ('programming? aargh - I cannot do that!'). And why should

    one be able to export to a bitmap with EXPORT in the first place, but

    not to DXF? This doesn't seem a logical choice. Better to make it clear

    and logical and nice and wonderful and let the user FIND that function

    easily...

     

    Andreas Weidner