Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Library management commands
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 1364 views
  • Users 0 members are here
  • copy
  • rename
  • library_editor
  • delete
Related

Library management commands

larsen
larsen over 14 years ago

I am evaluating the tool but after a short while of use I am having serious problems managing my self-made library.

 

How do I - inside a library:

 

Delete, Rename or Copy a: symbol, device or package?

 

It is _so_ easy to create new items (this has a prominent place in the select dialog), but it is difficult to rename or get rid of them again.

The remove/ rename command seems not to function or more likely I dont use it properly yet I follow the manual page 271. It fails saying that it cant find the item, yet it is there for sure.

 

Without this maintenace functionalty my library rapidly becomes messy and cloged up.

 

Hope for some hints.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    You don't say if you are using version 5.x or 6 - at least in version 5.12,

    if I open my library, click package and select the one I want to rename,

    this brings it up in the library editor window.  Then, if I click Library

    on the menu, the menu that comes up has a number of options.  Two of them

    are "Remove" and "Rename".  I have used both previously and they worked for

    me.  Have not tried it in 6 yet (still learning it myself - I have enough

    bugs without running into Eagle bugs  :lol:

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    You don't say if you are using version 5.x or 6 - at least in version 5.12,

    if I open my library, click package and select the one I want to rename,

    this brings it up in the library editor window.  Then, if I click Library

    on the menu, the menu that comes up has a number of options.  Two of them

    are "Remove" and "Rename".  I have used both previously and they worked for

    me.  Have not tried it in 6 yet (still learning it myself - I have enough

    bugs without running into Eagle bugs  :lol:

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Il 11/02/2012 07:10, Mike Fields ha scritto:

     

    You don't say if you are using version 5.x or 6 - at least in version 5.12,

    if I open my library, click package and select the one I want to rename,

    this brings it up in the library editor window.  Then, if I click Library

    on the menu, the menu that comes up has a number of options.  Two of them

    are "Remove" and "Rename".  I have used both previously and they worked for

    me.  Have not tried it in 6 yet (still learning it myself - I have enough

    bugs without running into Eagle bugs  :lol:

     

     

    I add here a question related to this topic.

     

    Is there a way to remove or move between libraries multiple components?

    I complain the lack of a interactive tree-view of the library(-ies)

    contents.

     

    It would be very handy to select multiple items and remove all together.

    Or move them to another library.

     

    Some time ago I spent several hours to remove one-by-one about one

    hundred of devices, symbols and packages while a multiple selection

    would have taken a couple of seconds.

     

    Please, consider to improve the library management. You should know that

    an electronic designer spends half time on the circuit and the other

    half on the libraries!

     

    Marco

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 11.02.2012 07:10, schrieb Mike Fields:

    if I open my library, click package and select the one I want to rename,

    this brings it up in the library editor window.  Then, if I click Library

    on the menu, the menu that comes up has a number of options.  Two of them

    are "Remove" and "Rename".

     

    Thanks for that information. I would NEVER, EVER have used these menu

    items, because I always thought they would remove or rename the LIBRARY.

     

    CadSoft: This is another example of insufficient menu item text. The

    menu item 'Library - Rename' SEEMS to mean 'rename library', because

    that's EXACTLY what it tells the user. What it really MEANS is 'rename

    device' or 'rename symbol' or 'rename package', so PLEASE put the

    additional word into the menu to clear things up.

     

    I've used EAGLE for 20 years and didn't know that this function was

    there due to this unclear menu wording. What a shame to both CadSoft and

    me...

     

    Andreas Weidner