EAGLE User Support (English) assign pan to mouse scroll
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
  • Replies 2 replies
  • Subscribers 177 subscribers
  • Views 295 views
  • Users 0 members are here
Related

assign pan to mouse scroll

autodeskguest
autodeskguest over 17 years ago

Hello,

 

I would like to assign actions for panning to the left/right and panning

up/down to "ctrl + scroll wheel" and "shift+ scroll wheel". I would also

like to remap the zoom function to "ctrl+shift + scroll wheel". Is this

possible? Can someone point me in the right direction as far as what

commands I should be looking at. I'm very new to eagle, but if I am

going to use this tool, I would really like an interface similar to dxp.

  I don't really care how much code I have to write to make this happen,

I just need to know that it is possible.

 

Thanks,

~Carl

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Morgan Leijström wrote:

    I do not know how to change Egale mouse actions, but if you are on Linux

    with an advanced mouse, take a look at btnx

    http://www.ollisalonen.com/btnx/ which works marvellous for my Logitexh

    Revolution.

     

    I also had problems with moving in alt grid until i found where in KDE

    settings i could turn of KDE grabbing that key combination.

     

    /Morgan

     

     

    This works great. I have setup btnx to map the scroll up and scroll down

    to F8 and F9, respectively, though you could in theory map it to

    whatever you wanted. However, after this I also had to use xmodmap to

    change the way X server relays these events:

     

    xmodmap -e "pointer 1 2 3 14 15 6 7 8 9 10 11 12 13 4 5"

     

    Then eagle receives scroll up and scroll down as F8 and F9. Now I use a

    script to assign specific commands to F8, C+F8 etc... However, how do I

    make the window pan to the right/left/up/down. Is there someway that I

    can reference the current window position in coordinates and then add a

    vector to it?

     

    Like I have seen examples of using "window" to pan to the mouse:

    Window (@);

     

    But I haven't seen anything referencing the current window.

     

    Thanks,

    ~Carl

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Morgan Leijström wrote:

    I do not know how to change Egale mouse actions, but if you are on Linux

    with an advanced mouse, take a look at btnx

    http://www.ollisalonen.com/btnx/ which works marvellous for my Logitexh

    Revolution.

     

    I also had problems with moving in alt grid until i found where in KDE

    settings i could turn of KDE grabbing that key combination.

     

    /Morgan

     

     

    This works great. I have setup btnx to map the scroll up and scroll down

    to F8 and F9, respectively, though you could in theory map it to

    whatever you wanted. However, after this I also had to use xmodmap to

    change the way X server relays these events:

     

    xmodmap -e "pointer 1 2 3 14 15 6 7 8 9 10 11 12 13 4 5"

     

    Then eagle receives scroll up and scroll down as F8 and F9. Now I use a

    script to assign specific commands to F8, C+F8 etc... However, how do I

    make the window pan to the right/left/up/down. Is there someway that I

    can reference the current window position in coordinates and then add a

    vector to it?

     

    Like I have seen examples of using "window" to pan to the mouse:

    Window (@);

     

    But I haven't seen anything referencing the current window.

     

    Thanks,

    ~Carl