Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 6 : unable to rename a via ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 1328 views
  • Users 0 members are here
Related

Eagle 6 : unable to rename a via ?

e14 Contributor
e14 Contributor over 14 years ago

Hi,

In Eagle V6.0.0, i was unable to rename a via, for example: I added a new via to the board and wanted to rename it as GND. I am used to do this in order to make ground planes connections in RF designs. With older versions of Eagle, there was no difficulty to do this.

Eagle 6.0.0 says: "Can not backannotate this operation. Please do this in the schematic!". But in the schematic, I don't know how to retrieve the via and rename it image

Could you advice how to do this with Eagle 6.0.0?

Thanks in advance.

 

Patrick

Sciensoria

User of Eagle v6.0.0 professionnal

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On Sat, 18 Feb 2012 22:42:23 +0000, patrick lafont wrote:

     

    Hi,

    In Eagle V6.0.0, i was unable to rename a via, for example: I added a

    new via to the board and wanted to rename it as GND. I am used to do

    this in order to make ground planes connections in RF designs. With

    older versions of Eagle, there was no difficulty to do this. Eagle 6.0.0

    says: "Can not backannotate this operation. Please do this in the

    schematic!". But in the schematic, I don't know how to retrieve the via

    and rename it image Could you advice how to do this with Eagle 6.0.0?

     

    In Eagle 5 I place my ground vias by name: instead of clicking on the

    "via" box, I go to the command line and type via 'gnd' (or via gnd -- I

    can't remember whether you need the quotes on that command).  Then all of

    the vias that I place are already on the ground net, and I don't have to

    mess with renaming them.

     

    I haven't used Eagle 6, but I sincerely hope that it works the same way.

     

    --

    Tim Wescott

    Control system and signal processing consulting

    www.wescottdesign.com

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks, Tim. This is a good idea. I try the command via 'gnd' and it works. The quotes are necessary.

     

    Patrick.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks, Tim. This is a good idea. I try the command via 'gnd' and it works. The quotes are necessary.

     

    Patrick.