Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 6 : unable to rename a via ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 1299 views
  • Users 0 members are here
Related

Eagle 6 : unable to rename a via ?

e14 Contributor
e14 Contributor over 14 years ago

Hi,

In Eagle V6.0.0, i was unable to rename a via, for example: I added a new via to the board and wanted to rename it as GND. I am used to do this in order to make ground planes connections in RF designs. With older versions of Eagle, there was no difficulty to do this.

Eagle 6.0.0 says: "Can not backannotate this operation. Please do this in the schematic!". But in the schematic, I don't know how to retrieve the via and rename it image

Could you advice how to do this with Eagle 6.0.0?

Thanks in advance.

 

Patrick

Sciensoria

User of Eagle v6.0.0 professionnal

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks, Tim. This is a good idea. I try the command via 'gnd' and it works. The quotes are necessary.

     

    Patrick.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On Sat, 18 Feb 2012 22:42:23 +0000, patrick lafont wrote:

     

    Hi,

    In Eagle V6.0.0, i was unable to rename a via, for example: I added a

    new via to the board and wanted to rename it as GND. I am used to do

    this in order to make ground planes connections in RF designs. With

    older versions of Eagle, there was no difficulty to do this. Eagle 6.0.0

    says: "Can not backannotate this operation. Please do this in the

    schematic!". But in the schematic, I don't know how to retrieve the via

    and rename it image Could you advice how to do this with Eagle 6.0.0?

     

    In Eagle 5 I place my ground vias by name: instead of clicking on the

    "via" box, I go to the command line and type via 'gnd' (or via gnd -- I

    can't remember whether you need the quotes on that command).  Then all of

    the vias that I place are already on the ground net, and I don't have to

    mess with renaming them.

     

    I haven't used Eagle 6, but I sincerely hope that it works the same way.

     

    --

    Tim Wescott

    Control system and signal processing consulting

    www.wescottdesign.com

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Il 19/02/2012 17:16, patrick lafont ha scritto:

     

    Thank you for your reply.

    I checked on the download area on Cadsoft web site, but they have only the 6.1.0 version. Where can I get the 6.1.2 ?

     

     

    http://www.cadsoftusa.com/betatest/

     

    Marco

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thank you for your reply.

    I checked on the download area on Cadsoft web site, but they have only the 6.1.0 version. Where can I get the 6.1.2 ?

    Regards

     

    Patrick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I placed the vias on the ground plane, but the via keeps his net which is automatically attributed. I would be happy to get the net name GND when placing the via on an existing ground plane. I did'nt know that.

     

    Patrick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Il 18/02/2012 23:42, patrick lafont ha scritto:

    Hi,

    In Eagle V6.0.0, i was unable to rename a via, for example: I added a new via to the board and wanted to rename it as GND. I am used to do this in order to make ground planes connections in RF designs. With older versions of Eagle, there was no difficulty to do this.

    Eagle 6.0.0 says: "Can not backannotate this operation. Please do this in the schematic!". But in the schematic, I don't know how to retrieve the via and rename it image

    Could you advice how to do this with Eagle 6.0.0?

     

     

    Are you sure the via has not already a signal's name?

    For example, it happens when you place a via on a net endpoint: the via

    gets the signal's name and you can't rename the via anymore (because

    you're renaming the whole signal and this cannot be done in layout).

     

    This applies to EAGLE V5 too.

    You have to ripup the via and placing it again.

     

    HTH

    Marco

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Am 18.02.2012 23:42, schrieb patrick lafont:

    Hi,

    In Eagle V6.0.0, i was unable to rename a via, for example: I added a new via to the board and wanted to rename it as GND. I am used to do this in order to make ground planes connections in RF designs. With older versions of Eagle, there was no difficulty to do this.

    Eagle 6.0.0 says: "Can not backannotate this operation. Please do this in the schematic!". But in the schematic, I don't know how to retrieve the via and rename it image

    Could you advice how to do this with Eagle 6.0.0?

    Thanks in advance.

     

    Patrick

    Sciensoria

    User of Eagle v6.0.0 professionnal

     

    You should update to ver.6.1.2 which has corrected lots of errors and at

    least there it works.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag