Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) custom pad shape creation
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 188 subscribers
  • Views 5973 views
  • Users 0 members are here
Related

custom pad shape creation

e14 Contributor
e14 Contributor over 14 years ago

Hi all,

 

I am trying to create a custom pad shape in Eagle 6.0. I have read many 'tutorials' on how to do so but I am still having problems. Hopefully someone here can point out where I am going wrong.

 

I start by making the shape I need using the polygon tool, then I insert an SMD pad into the polygon so that I have somewhere to route to (I just place a SMD pad after the polygon, no clever attachment).

At first this method seemed to work, but recently I have noticed that the autorouter sometimes routes tracks through the polygon as if it isn't there (creating a short). The polygon is on layer 1 as is the SMD pad.

 

Is there a way of making the entire polygon the pad?

 

.jpg's attached for clarification.

 

Thanks in advance for any help.

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Ok, I see that there is no way to turn a polygon into a pad. I have added tStop and tRestrict layers and that has solved most of the problems. However, when I export the Gerber files (using RS247X) all of my 'custom pad' shapes appear on the top layer, even though they are clearly set to the bottom layer. .jpg's attached for clarification.

     

    The component package was created on the top layer only. I can't see that this is a problem as the pads that are hidden inside the polygons do appear on the bottom layer, just the poly's that are wrong image

     

    hmm, seems I can attach a file so I will have to insert it ...

     

    imageimage

    I have checked the layer selections on the CAM processor and everything looks ok, .cmp = top, pads and vias. .sol = bottom, pads and vias.

     

    Once again, any help appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Ok, I see that there is no way to turn a polygon into a pad. I have added tStop and tRestrict layers and that has solved most of the problems. However, when I export the Gerber files (using RS247X) all of my 'custom pad' shapes appear on the top layer, even though they are clearly set to the bottom layer. .jpg's attached for clarification.

     

    The component package was created on the top layer only. I can't see that this is a problem as the pads that are hidden inside the polygons do appear on the bottom layer, just the poly's that are wrong image

     

    hmm, seems I can attach a file so I will have to insert it ...

     

    imageimage

    I have checked the layer selections on the CAM processor and everything looks ok, .cmp = top, pads and vias. .sol = bottom, pads and vias.

     

    Once again, any help appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    On 19.03.2012 11:39, b2lurk wrote:

    Ok, I see that there is no way to turn a polygon into a pad. I have added tStop and tRestrict layers and that has solved most of the problems. However, when I export the Gerber files (using RS247X) all of my 'custom pad' shapes appear on the top layer, even though they are clearly set to the bottom layer. .jpg's attached for clarification.

     

    The component package was created on the top layer only. I can't see that this is a problem as the pads that are hidden inside the polygons do appear on the bottom layer, just the poly's that are wrong image

     

    hmm, seems I can attach a file so I will have to insert it ...

     

      Image:eagle.JPG  Image:gerbv.JPG

    I have checked the layer selections on the CAM processor and everything looks ok, .cmp = top, pads and vias. .sol = bottom, pads and vias.

     

    Once again, any help appreciated.

     

     

     

     

     

    Hello,

     

    again the images didn't make it to the nntp forum.... I looked into the

    element14 page and checked the images there. I am not quite sure how you

    tried to define arbitrary pad shapes, the images don't have enough

    information for evaluation, but may I simply add a test taken from the

    EAGLE manual in order to explain how to do this....

     

     

    The typical way to draw an arbitrary pads shape is:

    - Place a PAD or SMD

    - Use POLYGON to draw the final pad shape

    - For a SMD typically in Layer Top

    - For a PAD you have to draw the final shape in all the layers you plan

        to use (Top, Bottom, Inner layers...)

    The PAD/SMDs center must be inside the polygon's area. Otherwise

    that polygon is not recognized as a part to the pad. Use a reasonable

    wire width for the polygon, which fulfils the Design Rules.

     

    - The alternative to POLYGON is WIRE

    Start the wire in the origin of the PAD/SMD. You have to draw this

    area in any signal layer you plan to use. Please use a reasonable wire

    width, which fits to the Design Rules.

    - Check the solder stop mask

    Mask data will be generated for the PAD/SMD area only. Display

    layers 29, tStop and 30, bStop. If you want to have the area not

    covered by solder stop lacquer, draw it manually in the appropriate

    layer(s).

    - Check the cream frame (solder paste mask)

    Display layers 31, tCream and 32, bCream for this. As we agreed upon

    defining packages always on the top side of a board, the layer we have

    to check is 31, tCream. Mask data will be generated automatically for

    the SMD area only. If this is not what you would like to have, simply

    draw the mask manually. Keep in mind that it is possible to switch off

    automatic generation of mask data in the SMD properties (Cream

    on/off).

     

     

    Concerning the layer problem: It mightbe the case that there is a

    problmem in EAGLE 6.0.0. You did not mention the version you are

    currently using, but I'ld recommend our current beta 6.1.3.

    ==> http://www.cadsoft.de/betatest/

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/