Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Component side on Double Sided PBC
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 190 subscribers
  • Views 754 views
  • Users 0 members are here
Related

Component side on Double Sided PBC

e14 Contributor
e14 Contributor over 14 years ago

I'm a new starter at pcb construction, but have used Eagle to successfuly design and make a single sided project board. I'm now designing a more complex double-sided board and have come up against a practical problem. The board will not have through hole plating, so I want to minimise soldering amongst the components.  I'm sure this is very commonly asked, but can I solder the components on either side? I have designed the board with a ground plane on both 'top' and 'bottom' layers. Looking at the pads, it will be far easier to locate all the components on the 'bottom' layer. There will be a few soldered connections on this side, but far fewer than if I put the components on the 'top' layer as defined by Eagle. Does it make any difference or am I missing a very obvious point?

Many thanks for you advice.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 03/11/2012 06:53 PM, waveguide wrote:

    I'm a new starter at pcb construction, but have used Eagle to successfuly design and make a single sided project board. I'm now designing a more complex double-sided board and have come up against a practical problem. The board will not have through hole plating, so I want to minimise soldering amongst the components.  I'm sure this is very commonly asked, but can I solder the components on either side? I have designed the board with a ground plane on both 'top' and 'bottom' layers. Looking at the pads, it will be far easier to manually solder all the components on the 'bottom' layer. There will be a few soldered connections necessary on the other side, but far fewer than if I put the components on the 'top' layer as defined by Eagle. Does it make any difference or am I missing a very obvious point?

    Many thanks for you advice.

     

    If you manually route you can control the connection side on part. You

    can also just edit and fix things after an autoroute. It is also

    possible to restrict traces from connecting to the top side of an IC by

    putting a box around the IC on the Trestrict layer. Look at the layer

    info on restrict and keepout

    The other way is to use smd to make the board much smaller and order the

    board for 1 off boards batchpcb.com was $10 + $2.50 per sq in for double

    sided with solder mask and 2 sided silk screen.

    Smd's are not much harder to hand solder. It just takes a fine temp

    controlled tip, magnification and a steady hand. I have used two irons

    to mount 0402 resistors and cap's. Just make sure the pads on the

    package extend enough to get the tip on the pad and pin at the same time.

    Paul R.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 03/11/2012 06:53 PM, waveguide wrote:

    I'm a new starter at pcb construction, but have used Eagle to successfuly design and make a single sided project board. I'm now designing a more complex double-sided board and have come up against a practical problem. The board will not have through hole plating, so I want to minimise soldering amongst the components.  I'm sure this is very commonly asked, but can I solder the components on either side? I have designed the board with a ground plane on both 'top' and 'bottom' layers. Looking at the pads, it will be far easier to manually solder all the components on the 'bottom' layer. There will be a few soldered connections necessary on the other side, but far fewer than if I put the components on the 'top' layer as defined by Eagle. Does it make any difference or am I missing a very obvious point?

    Many thanks for you advice.

     

    If you manually route you can control the connection side on part. You

    can also just edit and fix things after an autoroute. It is also

    possible to restrict traces from connecting to the top side of an IC by

    putting a box around the IC on the Trestrict layer. Look at the layer

    info on restrict and keepout

    The other way is to use smd to make the board much smaller and order the

    board for 1 off boards batchpcb.com was $10 + $2.50 per sq in for double

    sided with solder mask and 2 sided silk screen.

    Smd's are not much harder to hand solder. It just takes a fine temp

    controlled tip, magnification and a steady hand. I have used two irons

    to mount 0402 resistors and cap's. Just make sure the pads on the

    package extend enough to get the tip on the pad and pin at the same time.

    Paul R.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks for your help and insights. I'd still like to know whether it's OK to simply 'relabel' the Top and Bottom layers.

    Many thanks.