Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Component side on Double Sided PBC
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 190 subscribers
  • Views 749 views
  • Users 0 members are here
Related

Component side on Double Sided PBC

e14 Contributor
e14 Contributor over 14 years ago

I'm a new starter at pcb construction, but have used Eagle to successfuly design and make a single sided project board. I'm now designing a more complex double-sided board and have come up against a practical problem. The board will not have through hole plating, so I want to minimise soldering amongst the components.  I'm sure this is very commonly asked, but can I solder the components on either side? I have designed the board with a ground plane on both 'top' and 'bottom' layers. Looking at the pads, it will be far easier to locate all the components on the 'bottom' layer. There will be a few soldered connections on this side, but far fewer than if I put the components on the 'top' layer as defined by Eagle. Does it make any difference or am I missing a very obvious point?

Many thanks for you advice.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to auspoundy

    Now I have got my head around this issue, I can see that some components will and some components won't simply 'swap sides'. I've experimented with the mirror tool and I've also learned that the routing system in Eagle will allow you to prioritise the way connections are made. I found by altering the top and bottom routing signifiers (or whatever they are), the bias of the connections can be altered between sides.

    Many thanks for everyones' input.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • auspoundy
    0 auspoundy over 14 years ago

    For simple stuff, for example capacitors and resistors that have two pins, yes you can.  For more complex things, for instance a TO-220 package, you can as long as you carefully think about pin orientation.  For complex parts, usually the answer is no.  Take for example a 6-pin DIP IC, if you were to route to the pins, the intent of these pins would only match the IC orientation in one way, and swapping it's side would mean the pins are wired incorrectly.  So I would say in general, the more complex your circuit the more likely it is that you will need to put the device on the side you designed it on.

     

    But as others have said, just "mirror" the part and your orientation problems are solved.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • robotonics
    0 robotonics over 14 years ago in reply to e14 Contributor

    Hi

     

    If a part is on the top layer, and you wish it be on the bottom layer, then you only need to mirror the part.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • robotonics
    0 robotonics over 14 years ago in reply to e14 Contributor

    Hi

     

    If a part is on the top layer and use wish it be on the bottom layer then you only need to mirror the part.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks for your help and insights. I'd still like to know whether it's OK to simply 'relabel' the Top and Bottom layers.

    Many thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 03/11/2012 06:53 PM, waveguide wrote:

    I'm a new starter at pcb construction, but have used Eagle to successfuly design and make a single sided project board. I'm now designing a more complex double-sided board and have come up against a practical problem. The board will not have through hole plating, so I want to minimise soldering amongst the components.  I'm sure this is very commonly asked, but can I solder the components on either side? I have designed the board with a ground plane on both 'top' and 'bottom' layers. Looking at the pads, it will be far easier to manually solder all the components on the 'bottom' layer. There will be a few soldered connections necessary on the other side, but far fewer than if I put the components on the 'top' layer as defined by Eagle. Does it make any difference or am I missing a very obvious point?

    Many thanks for you advice.

     

    If you manually route you can control the connection side on part. You

    can also just edit and fix things after an autoroute. It is also

    possible to restrict traces from connecting to the top side of an IC by

    putting a box around the IC on the Trestrict layer. Look at the layer

    info on restrict and keepout

    The other way is to use smd to make the board much smaller and order the

    board for 1 off boards batchpcb.com was $10 + $2.50 per sq in for double

    sided with solder mask and 2 sided silk screen.

    Smd's are not much harder to hand solder. It just takes a fine temp

    controlled tip, magnification and a steady hand. I have used two irons

    to mount 0402 resistors and cap's. Just make sure the pads on the

    package extend enough to get the tip on the pad and pin at the same time.

    Paul R.