Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Component side on Double Sided PBC
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 190 subscribers
  • Views 753 views
  • Users 0 members are here
Related

Component side on Double Sided PBC

e14 Contributor
e14 Contributor over 14 years ago

I'm a new starter at pcb construction, but have used Eagle to successfuly design and make a single sided project board. I'm now designing a more complex double-sided board and have come up against a practical problem. The board will not have through hole plating, so I want to minimise soldering amongst the components.  I'm sure this is very commonly asked, but can I solder the components on either side? I have designed the board with a ground plane on both 'top' and 'bottom' layers. Looking at the pads, it will be far easier to locate all the components on the 'bottom' layer. There will be a few soldered connections on this side, but far fewer than if I put the components on the 'top' layer as defined by Eagle. Does it make any difference or am I missing a very obvious point?

Many thanks for you advice.

  • Sign in to reply
  • Cancel
Parents
  • auspoundy
    0 auspoundy over 14 years ago

    For simple stuff, for example capacitors and resistors that have two pins, yes you can.  For more complex things, for instance a TO-220 package, you can as long as you carefully think about pin orientation.  For complex parts, usually the answer is no.  Take for example a 6-pin DIP IC, if you were to route to the pins, the intent of these pins would only match the IC orientation in one way, and swapping it's side would mean the pins are wired incorrectly.  So I would say in general, the more complex your circuit the more likely it is that you will need to put the device on the side you designed it on.

     

    But as others have said, just "mirror" the part and your orientation problems are solved.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • auspoundy
    0 auspoundy over 14 years ago

    For simple stuff, for example capacitors and resistors that have two pins, yes you can.  For more complex things, for instance a TO-220 package, you can as long as you carefully think about pin orientation.  For complex parts, usually the answer is no.  Take for example a 6-pin DIP IC, if you were to route to the pins, the intent of these pins would only match the IC orientation in one way, and swapping it's side would mean the pins are wired incorrectly.  So I would say in general, the more complex your circuit the more likely it is that you will need to put the device on the side you designed it on.

     

    But as others have said, just "mirror" the part and your orientation problems are solved.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to auspoundy

    Now I have got my head around this issue, I can see that some components will and some components won't simply 'swap sides'. I've experimented with the mirror tool and I've also learned that the routing system in Eagle will allow you to prioritise the way connections are made. I found by altering the top and bottom routing signifiers (or whatever they are), the bias of the connections can be altered between sides.

    Many thanks for everyones' input.