Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Why does Eagle print everything "thicker"?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 1630 views
  • Users 0 members are here
  • eagle
  • problem
  • print
Related

Why does Eagle print everything "thicker"?

e14 Contributor
e14 Contributor over 14 years ago

I tried Eagle 5.11 on Windows XP, 6.1 on Mac Lion, and Windows XP.. Closed all layers but top layer.. The results are the same on Xerox 3140 printer.. Eagle prints everything a little thicker. The pads of MLF package bridges, and the 10mil lines between SO8 package's pins 1 and 2 tends to bridge to the pin 1.. The calibration is OK, I printed 100mm x 100mm rectangle and its good enough..

 

I printed to pdf, and printed the pdf with Preview application on macosx, this time the results are much better.. I would say "Oh, I can do that way" but after comparing it with the same packaging, same size that Proteus Ares produces, I saw that Proteus produces cleaner results.. It looks like Eagle widens everything..

 

Should I configure anything other than "calibrate" and "black" options on printer dialog?

 

Regards,

Deniz

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Deniz Can Cigsar wrote:

    I tried Eagle 5.11 on Windows XP, 6.1 on Mac Lion, and Windows XP..

    Closed all layers but top layer.. The results are the same on Xerox

    3140 printer.. Eagle prints everything a little thicker. The pads of

    MLF package bridges, and the 10mil lines between SO8 package's pins 1

    and 2 tends to bridge to the pin 1.. The calibration is OK, I printed

    100mm x 100mm rectangle and its good enough..

     

    I printed to pdf, and printed the pdf with Preview application on

    macosx, this time the results are much better.. I would say "Oh, I

    can do that way" but after comparing it with the same packaging, same

    size that Proteus Ares produces, I saw that Proteus produces cleaner

    results.. It looks like Eagle widens everything..

     

    Should I configure anything other than "calibrate" and "black"

    options on printer dialog?

     

    Regards,

    Deniz

     

     

    Some thoughts.

     

    Try a print to a printer with a higher resolution.

    The Xerox 3140 printer has a native resolution of 600 x 600

    The makes each dot 1.66 mil so and 5 mil trace could come out 6.4 mil (28%

    larger)

    An 8 mil trace would  be 8.3 mil. Closer but still over size.

     

    Those inkjet printing direct to copper laminate accept  1200 dpi  is

    required to get the detail faithfully.

     

    The width that a laser printer lays down is impacted by a number of factors;

    heat, pressure, amount of toner.

    You may have a darkness setting in your driver that if reduced may give the

    desired result as less toner is squashed out when it is set with heat and

    pressure.

     

    Proteus appears to do something different. Maybe it knows the printer

    resolution and thus has the ability to downsize an object so it does not

    grow larger than the design size when printed. It would then always be under

    size.

     

    I did a test print using an inkjet, replicating your "10mil lines between

    SO8 package's pins 1 and 2 tends to bridge to the pin 1"

    I get a  trace safely between the pins. But the clearances are less due to

    the wet ink spreading out on the surface. (High resolution on Photo glossy

    paper)

    With an MLF64 the ink spreading nearly closed the spaces between the pads.

    More so down the page than across. Again the printer affecting the outcome.

     

    To get a definitive answer as to where the size variation is being

    introduced and if whether Eagle does have an issue, a  test print and

    accurte measurement would be required.

     

    Hope this helps

    Warren

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Deniz Can Cigsar wrote:

    I tried Eagle 5.11 on Windows XP, 6.1 on Mac Lion, and Windows XP..

    Closed all layers but top layer.. The results are the same on Xerox

    3140 printer.. Eagle prints everything a little thicker. The pads of

    MLF package bridges, and the 10mil lines between SO8 package's pins 1

    and 2 tends to bridge to the pin 1.. The calibration is OK, I printed

    100mm x 100mm rectangle and its good enough..

     

    I printed to pdf, and printed the pdf with Preview application on

    macosx, this time the results are much better.. I would say "Oh, I

    can do that way" but after comparing it with the same packaging, same

    size that Proteus Ares produces, I saw that Proteus produces cleaner

    results.. It looks like Eagle widens everything..

     

    Should I configure anything other than "calibrate" and "black"

    options on printer dialog?

     

    Regards,

    Deniz

     

     

    Some thoughts.

     

    Try a print to a printer with a higher resolution.

    The Xerox 3140 printer has a native resolution of 600 x 600

    The makes each dot 1.66 mil so and 5 mil trace could come out 6.4 mil (28%

    larger)

    An 8 mil trace would  be 8.3 mil. Closer but still over size.

     

    Those inkjet printing direct to copper laminate accept  1200 dpi  is

    required to get the detail faithfully.

     

    The width that a laser printer lays down is impacted by a number of factors;

    heat, pressure, amount of toner.

    You may have a darkness setting in your driver that if reduced may give the

    desired result as less toner is squashed out when it is set with heat and

    pressure.

     

    Proteus appears to do something different. Maybe it knows the printer

    resolution and thus has the ability to downsize an object so it does not

    grow larger than the design size when printed. It would then always be under

    size.

     

    I did a test print using an inkjet, replicating your "10mil lines between

    SO8 package's pins 1 and 2 tends to bridge to the pin 1"

    I get a  trace safely between the pins. But the clearances are less due to

    the wet ink spreading out on the surface. (High resolution on Photo glossy

    paper)

    With an MLF64 the ink spreading nearly closed the spaces between the pads.

    More so down the page than across. Again the printer affecting the outcome.

     

    To get a definitive answer as to where the size variation is being

    introduced and if whether Eagle does have an issue, a  test print and

    accurte measurement would be required.

     

    Hope this helps

    Warren

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de