Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Why does Eagle print everything "thicker"?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 1622 views
  • Users 0 members are here
  • eagle
  • problem
  • print
Related

Why does Eagle print everything "thicker"?

e14 Contributor
e14 Contributor over 14 years ago

I tried Eagle 5.11 on Windows XP, 6.1 on Mac Lion, and Windows XP.. Closed all layers but top layer.. The results are the same on Xerox 3140 printer.. Eagle prints everything a little thicker. The pads of MLF package bridges, and the 10mil lines between SO8 package's pins 1 and 2 tends to bridge to the pin 1.. The calibration is OK, I printed 100mm x 100mm rectangle and its good enough..

 

I printed to pdf, and printed the pdf with Preview application on macosx, this time the results are much better.. I would say "Oh, I can do that way" but after comparing it with the same packaging, same size that Proteus Ares produces, I saw that Proteus produces cleaner results.. It looks like Eagle widens everything..

 

Should I configure anything other than "calibrate" and "black" options on printer dialog?

 

Regards,

Deniz

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Deniz,

     

    I was having the same issue while trying to manufacture a PCB with Presensitized PCBs.

     

    When I tried to print my design, I had the issue that a TQFP 100 IC had several Pads Shorted (due to the "thick" EAGLE printing), however by chance I came across a video tutorial in youtube on how to make an inverted board for negative presensitized PCBs.

     

    They Used the CAM Processor and chose Device to be "PS_INVERTED".

     

    I looked forward and there was a Device Called "PS", I used it like I was preparing the GERBER files (in this case I only checked the layers that are meant to be used) and it worked perfectly.

     

    I printed it with a 2400 dpi laser printer (which with the direct printing procedure draw me a lot of shorted pads) and there was no error.

     

    Try to do it that way, I'm pretty sure it will work this time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Guest wrote:

     

    Den 24/03/12 15.46, Deniz Can Cigsar skrev:

    I tried Eagle 5.11 on Windows XP, 6.1 on Mac Lion, and Windows XP.. Closed all layers but top layer.. The results are the same on Xerox 3140 printer.. Eagle prints everything a little thicker. The pads of MLF package bridges, and the 10mil lines between SO8 package's pins 1 and 2 tends to bridge to the pin 1.. The calibration is OK, I printed 100mm x 100mm rectangle and its good enough..

     

    I printed to pdf, and printed the pdf with Preview application on macosx, this time the results are much better.. I would say "Oh, I can do that way" but after comparing it with the same packaging, same size that Proteus Ares produces, I saw that Proteus produces cleaner results.. It looks like Eagle widens everything..

     

    Should I configure anything other than "calibrate" and "black" options on printer dialog?

     

     

    When i did toner-transfer PCB's i gave up using a 600 DPI printer.

     

    I bought an Samsung ML2580N which works wonders with toner transfer! -

    It has 1200 DPI resolution, so it's usable with finepitch components.

     

    Just my 2 cents.

     

    // Per.

     

     

    I am pretty sure it's not the resolution.. I did try 1200 dpi.. And also with 600dpi, using photo sensitive coating, with Proteus, I had really decent results.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Den 24/03/12 15.46, Deniz Can Cigsar skrev:

    I tried Eagle 5.11 on Windows XP, 6.1 on Mac Lion, and Windows XP.. Closed all layers but top layer.. The results are the same on Xerox 3140 printer.. Eagle prints everything a little thicker. The pads of MLF package bridges, and the 10mil lines between SO8 package's pins 1 and 2 tends to bridge to the pin 1.. The calibration is OK, I printed 100mm x 100mm rectangle and its good enough..

     

    I printed to pdf, and printed the pdf with Preview application on macosx, this time the results are much better.. I would say "Oh, I can do that way" but after comparing it with the same packaging, same size that Proteus Ares produces, I saw that Proteus produces cleaner results.. It looks like Eagle widens everything..

     

    Should I configure anything other than "calibrate" and "black" options on printer dialog?

     

     

    When i did toner-transfer PCB's i gave up using a 600 DPI printer.

     

    I bought an Samsung ML2580N which works wonders with toner transfer! -

    It has 1200 DPI resolution, so it's usable with finepitch components.

     

    Just my 2 cents.

     

    // Per.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    1. AFAIK CorelDraw cannot corret PS-data but you can edit them (ungroup/group).

    2. I did & I do lots of layouts with the PS_inverted output of the CAM-proc with EAGLE (from V2.6 on) & I had only (initial) probs with the global settings of the DRC. This was often mentioned in the forums, without no reaction from CadSoft :-(

    Thouhgt: check the diameter settings in the lbr(s). If they are at "auto" the global DRC rules apply. Changing them to a non-auto diameter will avoid this prob.

    HTH

    r

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Josef,

    It is more than what you mention.. Just put MLF32 on the board and print.. You'll see all the pads will stick together.. The error is more than 0.3mm, which is nothing for a laser printer.. But PS might work if Corell Draw has a correction for that.. Has it?

     

    Tim,

    Than it is pity, because it is another thing they didn't pay attention..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    On Sun, 25 Mar 2012 16:39:10 +1200, Warren Brayshaw wrote:

     

    Deniz Can Cigsar wrote:

    >> I process prototypes myself using photosensitives.. There isn't "one

    >> day shipment" choise here.. Because of that I need decent printouts as

    >> I am using small packages.

    >>

    >> I've been working with Proteus without an issue, however this was

    >> surprize to me..

     

    After re-reading Tim's suggestion to print from a Gerber viewer I

    printed from gerbv

    The print is far more realistic (better) than that of Eagles print

    function

     

    Today's small geometries and printer resolutions seem to be showing up a

    deficiency in Eagles code.

    Perhaps its time for Cadsoft to revisit the printing code. Good spotting

    Deniz

     

    Perhaps the folks at Eagle view the printer stuff as mere documentation

    (as do I), and don't lavish it with the attention you'd need if you were

    seriously using it to generate artwork.

     

    I frankly don't know if that's the right attitude or not -- but I've

    never, ever, seen their Gerbers go astray.

     

    --

    Tim Wescott

    Control system and signal processing consulting

    www.wescottdesign.com

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thank you Warren..

     

    I forgot to mention that I tried 1200dpi.. The result was the same.. What I think is, on printing directly to the printer, it looks like Eagle uses line drawing routins with some thickness given.. However, PDF and PS are vector formats and the actual drawing is done by the viewer..

     

    I think I'll stick with Proteus.. I didn't liked Eagles libraries, and started redesigning, until I came across the problem.. Most of the components were designed for wave soldering but reflow..

     

    It's also interesting that the PCB software have not advanced much since 1990's.. I still don't see a good candidate to replace "BoardMaker" of those days..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Try to print (postscript)negative with the CAM-job, then import the file

    into CorelDraw with the option "ps interpreted",  there will be not such an

    issue. In german it's called "Tonwertzuwachs" for laser- & inkjet-printers

    (I found no english expression for this word, but it's the same as Warren

    found out) for printing positive layouts.

    r

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Deniz Can Cigsar wrote:

    I process prototypes myself using photosensitives.. There isn't "one

    day shipment" choise here.. Because of that I need decent printouts

    as I am using small packages.

     

    I've been working with Proteus without an issue, however this was

    surprize to me..

     

    After re-reading Tim's suggestion to print from a Gerber viewer I printed

    from gerbv

    The print is far more realistic (better) than that of Eagles print function

     

    Today's small geometries and printer resolutions seem to be showing up a

    deficiency in Eagles code.

    Perhaps its time for Cadsoft to revisit the printing code.

    Good spotting Deniz

     

    Warren

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Deniz Can Cigsar wrote:

    I tried Eagle 5.11 on Windows XP, 6.1 on Mac Lion, and Windows XP..

    Closed all layers but top layer.. The results are the same on Xerox

    3140 printer.. Eagle prints everything a little thicker. The pads of

    MLF package bridges, and the 10mil lines between SO8 package's pins 1

    and 2 tends to bridge to the pin 1.. The calibration is OK, I printed

    100mm x 100mm rectangle and its good enough..

     

    I printed to pdf, and printed the pdf with Preview application on

    macosx, this time the results are much better.. I would say "Oh, I

    can do that way" but after comparing it with the same packaging, same

    size that Proteus Ares produces, I saw that Proteus produces cleaner

    results.. It looks like Eagle widens everything..

     

    Should I configure anything other than "calibrate" and "black"

    options on printer dialog?

     

    Regards,

    Deniz

     

     

    Some thoughts.

     

    Try a print to a printer with a higher resolution.

    The Xerox 3140 printer has a native resolution of 600 x 600

    The makes each dot 1.66 mil so and 5 mil trace could come out 6.4 mil (28%

    larger)

    An 8 mil trace would  be 8.3 mil. Closer but still over size.

     

    Those inkjet printing direct to copper laminate accept  1200 dpi  is

    required to get the detail faithfully.

     

    The width that a laser printer lays down is impacted by a number of factors;

    heat, pressure, amount of toner.

    You may have a darkness setting in your driver that if reduced may give the

    desired result as less toner is squashed out when it is set with heat and

    pressure.

     

    Proteus appears to do something different. Maybe it knows the printer

    resolution and thus has the ability to downsize an object so it does not

    grow larger than the design size when printed. It would then always be under

    size.

     

    I did a test print using an inkjet, replicating your "10mil lines between

    SO8 package's pins 1 and 2 tends to bridge to the pin 1"

    I get a  trace safely between the pins. But the clearances are less due to

    the wet ink spreading out on the surface. (High resolution on Photo glossy

    paper)

    With an MLF64 the ink spreading nearly closed the spaces between the pads.

    More so down the page than across. Again the printer affecting the outcome.

     

    To get a definitive answer as to where the size variation is being

    introduced and if whether Eagle does have an issue, a  test print and

    accurte measurement would be required.

     

    Hope this helps

    Warren

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>