Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Why does Eagle print everything "thicker"?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 1626 views
  • Users 0 members are here
  • eagle
  • problem
  • print
Related

Why does Eagle print everything "thicker"?

e14 Contributor
e14 Contributor over 14 years ago

I tried Eagle 5.11 on Windows XP, 6.1 on Mac Lion, and Windows XP.. Closed all layers but top layer.. The results are the same on Xerox 3140 printer.. Eagle prints everything a little thicker. The pads of MLF package bridges, and the 10mil lines between SO8 package's pins 1 and 2 tends to bridge to the pin 1.. The calibration is OK, I printed 100mm x 100mm rectangle and its good enough..

 

I printed to pdf, and printed the pdf with Preview application on macosx, this time the results are much better.. I would say "Oh, I can do that way" but after comparing it with the same packaging, same size that Proteus Ares produces, I saw that Proteus produces cleaner results.. It looks like Eagle widens everything..

 

Should I configure anything other than "calibrate" and "black" options on printer dialog?

 

Regards,

Deniz

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On Sat, 24 Mar 2012 14:46:01 +0000, Deniz Can Cigsar wrote:

     

    I tried Eagle 5.11 on Windows XP, 6.1 on Mac Lion, and Windows XP..

    Closed all layers but top layer.. The results are the same on Xerox 3140

    printer.. Eagle prints everything a little thicker. The pads of MLF

    package bridges, and the 10mil lines between SO8 package's pins 1 and 2

    tends to bridge to the pin 1.. The calibration is OK, I printed 100mm x

    100mm rectangle and its good enough..

     

    I printed to pdf, and printed the pdf with Preview application on

    macosx, this time the results are much better.. I would say "Oh, I can

    do that way" but after comparing it with the same packaging, same size

    that Proteus Ares produces, I saw that Proteus produces cleaner

    results.. It looks like Eagle widens everything..

     

    Should I configure anything other than "calibrate" and "black" options

    on printer dialog?

     

    Regards,

    Deniz

     

    Eagle "prints" just fine to Gerber files, which is what you send off to

    the circuit board house.

     

    If you need accurate pdf files, perhaps you should see if you can find a

    Gerber file viewer that prints?

     

    --

    My liberal friends think I'm a conservative kook.

    My conservative friends think I'm a liberal kook.

    Why am I not happy that they have found common ground?

     

    Tim Wescott, Communications, Control, Circuits & Software

    http://www.wescottdesign.com

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I process prototypes myself using photosensitives.. There isn't "one day shipment" choise here.. Because of that I need decent printouts as I am using small packages.

     

    I've been working with Proteus without an issue, however this was surprize to me..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Deniz Can Cigsar wrote:

    I process prototypes myself using photosensitives.. There isn't "one

    day shipment" choise here.. Because of that I need decent printouts

    as I am using small packages.

     

    I've been working with Proteus without an issue, however this was

    surprize to me..

     

    After re-reading Tim's suggestion to print from a Gerber viewer I printed

    from gerbv

    The print is far more realistic (better) than that of Eagles print function

     

    Today's small geometries and printer resolutions seem to be showing up a

    deficiency in Eagles code.

    Perhaps its time for Cadsoft to revisit the printing code.

    Good spotting Deniz

     

    Warren

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    1. AFAIK CorelDraw cannot corret PS-data but you can edit them (ungroup/group).

    2. I did & I do lots of layouts with the PS_inverted output of the CAM-proc with EAGLE (from V2.6 on) & I had only (initial) probs with the global settings of the DRC. This was often mentioned in the forums, without no reaction from CadSoft :-(

    Thouhgt: check the diameter settings in the lbr(s). If they are at "auto" the global DRC rules apply. Changing them to a non-auto diameter will avoid this prob.

    HTH

    r

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    1. AFAIK CorelDraw cannot corret PS-data but you can edit them (ungroup/group).

    2. I did & I do lots of layouts with the PS_inverted output of the CAM-proc with EAGLE (from V2.6 on) & I had only (initial) probs with the global settings of the DRC. This was often mentioned in the forums, without no reaction from CadSoft :-(

    Thouhgt: check the diameter settings in the lbr(s). If they are at "auto" the global DRC rules apply. Changing them to a non-auto diameter will avoid this prob.

    HTH

    r