Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Creating new parts - copy and paste?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 723 views
  • Users 0 members are here
  • library
  • create_a_part
Related

Creating new parts - copy and paste?

e14 Contributor
e14 Contributor over 14 years ago

Is there some way to simply open an existing device with the same footprint as your new device and copy the whole enchilada and paste it into your new device and then just edit the pin names and be done with it?  If there is a way, can someone tell me what it is?  And if there isn't, why not?   It seems like this would be the ideal and simplest solution for 99% of every new device one wanted to add to their library.  Or am I missing something?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Op Sun, 01 Apr 2012 01:06:43 +0200 schreef Don French 

    <noreply-101094@element14.com>:

     

    Or am I missing something?

     

     

    It depends...

     

    You don't say what version you are using, with 4.0 copy & paste it is, but 

    I'll assume it's 5.x or higher. In that case:

     

    1) open the library you want to add the device to

    2) find the device you want to copy in the 'control panel'

    3) right click on the device and select 'copy to library'

     

    that's it! start modifying your enchilada ...

     

     

    Richard

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Well that kind of worked. 

     

    I am using 5.5 and am using it for the first time in a very long time - and I never did much library management or part creation when I did use it.  The problem now is that it copied the part to my library but it did not offer  the chance to change the name so now the part I want to use has a completely inappropriate name.  Also, the part I wanted to copy is one of several at the second of the part hierarchy and it only allowed me to copy the top level so I got about 20 parts that I don't want.  I am sure that there must be a way to correct this but I do not find a way to move my new part up to the first level in the hierarchy of my library or to rename it with an appropriate name.  

     

    Wouldn't it be better if there were a menu option to create a new part from an existing part and prompt you to name your new part at that time?    I am feeling frustrated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    That last post should have said at the second *level* of the hierarchy. 

     

    Why isn't there a library that  just contains generic packages? Or is there?  I wish Eagle Cad have the option of creating a part from a standard package like MSOP and then prompt you for everything that need to be set like Value, Description, Source, Pin names.  Well, OK, forgetting about re-designing Eagle Cad, at least it could come with a library of generic packages that one could right-click on (ahem - intuitive, that) to begin making a new part. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Don French wrote:

    >........................................................... Well, OK,

    forgetting about re-designing Eagle Cad, at least it could come with

    a library of generic packages that one could right-click on (ahem -

    intuitive, that) to begin making a new part.

     

    It does, See ref-packages.lbr and ref-packages-longpad.lbr

    Find the package of interest, right click and Copy to library (Your library

    that you opened prior to this to ready it for receiving  devices and

    packages from Control Panel.)

     

    Then continue to make the new part as explained in the many tutorials

    available

     

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Don French wrote:

    >........................................................... Well, OK,

    forgetting about re-designing Eagle Cad, at least it could come with

    a library of generic packages that one could right-click on (ahem -

    intuitive, that) to begin making a new part.

     

    It does, See ref-packages.lbr and ref-packages-longpad.lbr

    Find the package of interest, right click and Copy to library (Your library

    that you opened prior to this to ready it for receiving  devices and

    packages from Control Panel.)

     

    Then continue to make the new part as explained in the many tutorials

    available

     

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de