I found the part I needed in the part listing on Cadsoft Eagle. It shows the proper amount of pins on the board view but
doesn't have all of the connections needed on the schematic view. This is probably a noob question but either my googlefu is weak or
there isn't any info regarding this... or the question is so stupid nobody bothers to ask it. 
Below are two example I found in the components list. Both are 16 pin monostable multivibrators but no all of the pins are listed on the schematic view.