Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) DRC vRestrict not honored in linux 5.1.0
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 484 views
  • Users 0 members are here
Related

DRC vRestrict not honored in linux 5.1.0

holla2040
holla2040 over 18 years ago

Folks,

The 5.1.0 manual page 145 says "vRestrict regions are not examined by the

DRC".

 

I'm creating a package with in-board heatsink with a top layer and bottom

layer poly regions connected via pads (TI called this a PowerPAD). I

surround my poly/pad setup with a vRestrict poly. The DRC reports clearance

errors with the "DRC/Misc/Check Restrict" option enabled or disabled.

 

Is the page 145 description correct and I'm just doing something wrong?

 

Thanks,

Craig

ps. sorry for the cross-posting, I send the original to the wrong group.

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 18 years ago

    Craig Hollabaugh schrieb:

    I'm creating a package with in-board heatsink with a top layer and

    bottom

    layer poly regions connected via pads (TI called this a PowerPAD). I

    surround my poly/pad setup with a vRestrict poly. The DRC reports

    clearance

    errors with the "DRC/Misc/Check Restrict" option enabled or disabled.

     

    Is the page 145 description correct and I'm just doing something wrong?

    The manual wants to say that the DRC does not check for vias that

    are placed inside the ViaRestrict area. Placing a via inside the

    area manually won't be indicated by an error message.

    Only the Autorouter will take care of such areas and won't

    place vias inside.

     

    Richard,

    Thanks for writing. I can't place vias within a package (or at least I don't

    know how to). I think I can do all this on a board because I can assign a

    signal to the top side poly, bottom side poly and the via then they're all

    connected. However I can't figure out how to create these pieces within a

    library package because I can't assign a signal to a poly or use vias. Do

    you see my problem?

    Craig

     

    You said placing a manually placing a via the area won't generate an error

    message if in vRestrict.

     

     

    You misunderstood my words:

    The vRestrict area can be used for the autorouter. If you draw this

    area in the layout, the autorouter is not allowed to set vias inside.

    In case you set vias manually in the layout and there is a vRestrict

    area that covers the vias, the DRC does not complain about the vias

    inside the vRestrict area.

     

    Concerning package design:

    You are right, there is no via command in the package editor. And it

    is not possible to name, for example, polygons there.

    But in some cases it is neccessary to use a polygon, for example,

    for a special pad shape. In this case you can combine polygon and

    Smds or Pads. But you will get an DRC error in the Layout which you

    can approve then. There is no other solution at the moment.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 18 years ago

    Craig Hollabaugh schrieb:

    I'm creating a package with in-board heatsink with a top layer and

    bottom

    layer poly regions connected via pads (TI called this a PowerPAD). I

    surround my poly/pad setup with a vRestrict poly. The DRC reports

    clearance

    errors with the "DRC/Misc/Check Restrict" option enabled or disabled.

     

    Is the page 145 description correct and I'm just doing something wrong?

    The manual wants to say that the DRC does not check for vias that

    are placed inside the ViaRestrict area. Placing a via inside the

    area manually won't be indicated by an error message.

    Only the Autorouter will take care of such areas and won't

    place vias inside.

     

    Richard,

    Thanks for writing. I can't place vias within a package (or at least I don't

    know how to). I think I can do all this on a board because I can assign a

    signal to the top side poly, bottom side poly and the via then they're all

    connected. However I can't figure out how to create these pieces within a

    library package because I can't assign a signal to a poly or use vias. Do

    you see my problem?

    Craig

     

    You said placing a manually placing a via the area won't generate an error

    message if in vRestrict.

     

     

    You misunderstood my words:

    The vRestrict area can be used for the autorouter. If you draw this

    area in the layout, the autorouter is not allowed to set vias inside.

    In case you set vias manually in the layout and there is a vRestrict

    area that covers the vias, the DRC does not complain about the vias

    inside the vRestrict area.

     

    Concerning package design:

    You are right, there is no via command in the package editor. And it

    is not possible to name, for example, polygons there.

    But in some cases it is neccessary to use a polygon, for example,

    for a special pad shape. In this case you can combine polygon and

    Smds or Pads. But you will get an DRC error in the Layout which you

    can approve then. There is no other solution at the moment.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • holla2040
    holla2040 over 10 years ago in reply to Richard_H

    Richard,

     

    I'm confused. I asked this question about 8 years ago in 2008. Did you just answer this now, on April 7th? Or is there a problem with the e14 forum?

     

    Is the answer still valid for the current version of eagle?

     

    Craig