Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Schematic-vs-PCB Differences
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 188 subscribers
  • Views 828 views
  • Users 0 members are here
  • board
  • pcb_traces
  • autorouter
  • schematic
Related

Schematic-vs-PCB Differences

e14 Contributor
e14 Contributor over 14 years ago

I am having a problem with connections on the schematic not following through to become nets on the layout drawing. Is this a common problem with EAGLE? I am using a standard library part and a part that I created, so it is possible that my part will simply not connect to the net. I had no problem making the connection on the schematic, though, so I don't understand why it doesn't connect on the PCB.

 

Any help would be appreciated.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

     

    "Paul Horst" <noreply-105171@element14.com> wrote in message

    news:1807090506.20961338302985506.JavaMail.jive@flmspu-csapp-02.premierfarnell.com...

    >I am having a problem with connections on the schematic not following

    >through to become nets on the layout drawing. Is this a common problem with

    >EAGLE? I am using a standard library part and a part that I created, so it

    >is possible that my part will simply not connect to the net. I had no

    >problem making the connection on the schematic, though, so I don't

    >understand why it doesn't connect on the PCB.

     

    Any help would be appreciated.

     

    Probably not the source of your problem but if you turn off connection dots

    in control panel, Eagle does not take the same care in making sure that

    wires butted up against each other will get connected. Connections are more

    hap-hazard than if you throw down a connection dot.  It makes me feel like

    odd-man-out but I absolutely refuse to have those horrendous oversize

    connection dots cluttering up my schematic. Must run ERC from time-to time

    but the issue is not really very seriously treated according to Eagle (huh

    really!). Make sure that messages like "Close but unconnected wires in nets

    n$1 and n$1, do not go ignored.

     

    In the schematic editor, select Options || Misc || Auto set junction

    (junction, meaning the dot).

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Paul Horst wrote:

     

    >I am having a problem with connections on the schematic not following through to become nets on

    >the layout drawing. Is this a common problem with EAGLE? I am using a standard library part and>

    >a part that I created, so it is possible that my part will simply not connect to the net. I had no

    >problem making the connection on the schematic, though, so I don't understand why it doesn't

    >connect on the PCB.

     

    are you sure board and schematic are still consistent?

    Consitency may be lost if you change the schematic (adding/deleting

    parts/nets is relevant, just moving things around is not a problem)

    while the board file is closed.

    Run ERC to check.

     

    I don't think wire vs. net command is an issue here.

    The main difference between wire and net commands is the fact that the

    net command will place connection points automatically, where the wire

    command does not (so a connection and a crossing lock to same).

     

    The easiest way to see if nets/wires are connected to a part is to

    pick up the part and move it. All connected nets will follow the part

    in that case (use ESC to abort the move without modifications).

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    On 5/29/2012 10:18 AM, Paul Horst wrote:

    Thanks, Doug. I checked the connections on the schematic like you suggested and the connections are solid. I have been using the wire tool to make all of my connections, though. Should I be using the net tool instead? I tried using it to replace the connection in question, but it won't connect to my part. This is a part that I created myself, so there is a distinct possibility that I made a mistake on it. I am trying to connect to an output pin that I created as an output on the symbol.

     

    Thanks again,

     

    Paul

     

     

     

    Yes, you should be using the net tool for connections.

    Not intuitive, but once you know it is ok.

     

    The most likely issue is the grid being different between the library

    part and the schematic. Check the grid on the part and compare it to

    what is on the schematic.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks, Doug. I checked the connections on the schematic like you suggested and the connections are solid. I have been using the wire tool to make all of my connections, though. Should I be using the net tool instead? I tried using it to replace the connection in question, but it won't connect to my part. This is a part that I created myself, so there is a distinct possibility that I made a mistake on it. I am trying to connect to an output pin that I created as an output on the symbol.

     

    Thanks again,

     

    Paul

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 5/29/2012 7:49 AM, Paul Horst wrote:

    I am having a problem with connections on the schematic not following through to become nets on the layout drawing. Is this a common problem with EAGLE? I am using a standard library part and a part that I created, so it is possible that my part will simply not connect to the net. I had no problem making the connection on the schematic, though, so I don't understand why it doesn't connect on the PCB.

     

    Any help would be appreciated.

     

     

    If the grid is different between the part and the schematic it may look

    connected but not be. You can adjust the grid or set an alternate grid

    for this.

    If you grab the wire near the connection and it moves by itself then it

    is not connected. Another common thing is if one uses wire instead of

    net to make connections,

     

     

    -D

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer