Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Schematic-vs-PCB Differences
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 188 subscribers
  • Views 830 views
  • Users 0 members are here
  • board
  • pcb_traces
  • autorouter
  • schematic
Related

Schematic-vs-PCB Differences

e14 Contributor
e14 Contributor over 14 years ago

I am having a problem with connections on the schematic not following through to become nets on the layout drawing. Is this a common problem with EAGLE? I am using a standard library part and a part that I created, so it is possible that my part will simply not connect to the net. I had no problem making the connection on the schematic, though, so I don't understand why it doesn't connect on the PCB.

 

Any help would be appreciated.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 5/29/2012 7:49 AM, Paul Horst wrote:

    I am having a problem with connections on the schematic not following through to become nets on the layout drawing. Is this a common problem with EAGLE? I am using a standard library part and a part that I created, so it is possible that my part will simply not connect to the net. I had no problem making the connection on the schematic, though, so I don't understand why it doesn't connect on the PCB.

     

    Any help would be appreciated.

     

     

    If the grid is different between the part and the schematic it may look

    connected but not be. You can adjust the grid or set an alternate grid

    for this.

    If you grab the wire near the connection and it moves by itself then it

    is not connected. Another common thing is if one uses wire instead of

    net to make connections,

     

     

    -D

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks, Doug. I checked the connections on the schematic like you suggested and the connections are solid. I have been using the wire tool to make all of my connections, though. Should I be using the net tool instead? I tried using it to replace the connection in question, but it won't connect to my part. This is a part that I created myself, so there is a distinct possibility that I made a mistake on it. I am trying to connect to an output pin that I created as an output on the symbol.

     

    Thanks again,

     

    Paul

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks, Doug. I checked the connections on the schematic like you suggested and the connections are solid. I have been using the wire tool to make all of my connections, though. Should I be using the net tool instead? I tried using it to replace the connection in question, but it won't connect to my part. This is a part that I created myself, so there is a distinct possibility that I made a mistake on it. I am trying to connect to an output pin that I created as an output on the symbol.

     

    Thanks again,

     

    Paul

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    On 5/29/2012 10:18 AM, Paul Horst wrote:

    Thanks, Doug. I checked the connections on the schematic like you suggested and the connections are solid. I have been using the wire tool to make all of my connections, though. Should I be using the net tool instead? I tried using it to replace the connection in question, but it won't connect to my part. This is a part that I created myself, so there is a distinct possibility that I made a mistake on it. I am trying to connect to an output pin that I created as an output on the symbol.

     

    Thanks again,

     

    Paul

     

     

     

    Yes, you should be using the net tool for connections.

    Not intuitive, but once you know it is ok.

     

    The most likely issue is the grid being different between the library

    part and the schematic. Check the grid on the part and compare it to

    what is on the schematic.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer