Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) First time experience / Why is this not as expected
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 189 subscribers
  • Views 561 views
  • Users 0 members are here
Related

First time experience / Why is this not as expected

e14 Contributor
e14 Contributor over 14 years ago

I am starting an electronics workshop for young kids, primarily revolving around microcontrollers, using SMD components with a 1.27mm pitch. As part of the program I will be introducing them to PCB software. The youngsters are eager, impatient and intuitive. I downloaded Eagle 6.2.0/Lite and tried a simple design and here are my experiences.

 

I worked with Eagle 4.0 more than 10 years ago and have forgotten nearly everything so this will be a trip through memory lane, so practically I am novice with deja vu.

 

The test design consists of a PIC16F648A-E/PPIC16F648A-E/P, 10 Leds, 2 Hall detectors, a bunch of resistors and a 6 pin connector.

 

- Placing the main component was straight forward. Also the power supply lines and symbols.

- Next I want to place the leds and bump into the first serious problem. The led is SMD with a 2mm by 1.25mm package.

 

The add component displays a staggering amount of candidates, this was to be expected. What was not to be expected that it is virtually impossible to make a generic selection. The selection box is very manufacture/part-number orientated. I miss a couple of section options including package type. I randomly browse through the list, and see "0805". I associate this with a resistor package and assume it is correct.

 

- Next I place the resistors. After some tries, I notice that the magic search string is "*0805*".

- Next I need to place the Hall detectors. I browse through the list and find the SIP3 package.

- Next I need to place the connector.

 

The connector is a single row, 1.27mm pitch 6 pin connector. I type "connector" in the search. The list is too long to work with. I do not have a brand name or part number to narrow the selection. After a couple of minutes I abandon randomly walking through the list and decide to browse through all the library components for a visual match. Some are good candidates but as there are no dimensions in the description. Selecting a few show that they are all the wrong size. Abandoning that I go to my component suppliers site to search for a matching

manufacture/part-number. None are present in the library, After more than 30 minutes I give up and just select one, knowing that the size is incorrect.

 

- I complete the schematic and switch to the board component placer.

- All the components are located under each other.

 

I pick up the first to move to a better location and get:

"The light edition of Eagle cannot perform action. Some objects extend outside allowed board area".

No board edge is shown so I do not know where the boundary lies.

I assume you need to set the board size somewhere, but I cannot find any menu item that suggests this.

The help does not offer any solution.

 

After a two hour session I give up and start writing this posting.

 

I truly admire Eagle and the capabilities. I do not understand why I cannot place the components on the board in the Lite version. But the component selection screen lacks too many selection tools -- In this case being package type, dimension sizes, pitch, and for the #rows/#pins. I get my stuff from RS-components/Mouser and Farnell, they have the selection tools I was expecting to see. There are just too many components to select on manufacture/part-number/description only, especially when they are incomplete.

 

The controls of Eagle are reasonably intuitive. But sadly, at this moment I cannot use Eagle for the PCB workshop. Placing of the components is locked, I was not able to try the auto-router, and I cannot expect the kids to spend ages just on finding and selecting the components.

  • Sign in to reply
  • Cancel
Parents
  • skyflyrr
    0 skyflyrr over 14 years ago

    Hello all, I would like to say that I completely agree with this psot. I too am new to Eagle and though I have the professional version with almost no limitations, the library is a serious problem. While it may seem that having actual components to every possible part that exists is good, in actual use it is a nightmare. A generic library with several hundred components and their packages is by far much better. Eagle is great, but sorely lacking in a way to use the library in a quick and efficient manner. Please consider adding a generic library which contains through-hole and smd components and packages or at minimum a way to build packages in a quick and efficient manner. It should take minutes to build a package with any size pad, number of pads and pitch without having to constantly change grid size or copy pads to complete a high pad count package. If Eagle already has this capability I would appreciate someone letting me know.

     

    Thank you,

     

    Bob Moreno

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to skyflyrr

    Am 27.06.2012 16:48, schrieb Bob Moreno:

    the library is a serious problem. While it may seem that having actual

    > components to every possible part that exists is good, in actual use

    it is

    > a nightmare.

     

    Yes. Unfortunately, this is the case with ALL such programs. EAGLE at

    least provides SOME descriptions, other programs don't even do THAT.

     

    Additionally, ALL libraries are sorted by manufacturer: This is the only

    DECENT possibility the software programmers can do. Unfortunately, the

    manufacturer is most often what the users do NOT care about - they just

    want a device that's correct in footprint. And since footprints for

    connectors do NOT have any predefined name that is used all over the

    world, the user doesn't even know what to search for.

     

    And still worse: If, after years of searching, you DO find the right

    device, you might also find (after building the board, which didn't

    work) that there is some error in the library.

     

    Therefore: Whatever CAD program you're using, the FIRST thing you should

    learn is how to create your own libraries. Only in the most dire

    circumstances we use other people's libraries here. I myself spend just

    below 10% of my time creating EAGLE parts (but that's for about 20

    users). Of course that's all a lot of work, but it's the only

    possibility to get what YOU can work with easily. And, in the end,

    creating a part is often NOT more work than searching hours for the

    correct library device.

     

    A generic library with several hundred components and their packages

    > is by far much better.

     

    Yes. And since everybody has DIFFERENT library needs, everybody (or at

    least the EAGLE administrator) should build their own libraries.

     

    It should take minutes to build a package with any size pad,

    > number of pads and pitch without having to constantly change grid size

    > or copy pads to complete a high pad count package.

     

    Creating most through-hole devices DOES only take minutes, but for SMDs

    with their strange pad positions, which often do not even use the same

    grid in both directions, this is NOT nice. But here, the culprit is not

    EAGLE, but the component manufacturers, who think up designs that just

    ARE very complicated.

     

    True, EAGLE's library capabilities COULD be improved. There might even

    now exist some ULPs that help you in this respect, but I don't know

    them, and they're not available in the GUI, so new users will never find

    that functionality. But overall, I have the impression that only about

    30% of the library problems are CadSoft's, the other 70% are different

    user desires, strange manufacturer's designs,...

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to skyflyrr

    Am 27.06.2012 16:48, schrieb Bob Moreno:

    the library is a serious problem. While it may seem that having actual

    > components to every possible part that exists is good, in actual use

    it is

    > a nightmare.

     

    Yes. Unfortunately, this is the case with ALL such programs. EAGLE at

    least provides SOME descriptions, other programs don't even do THAT.

     

    Additionally, ALL libraries are sorted by manufacturer: This is the only

    DECENT possibility the software programmers can do. Unfortunately, the

    manufacturer is most often what the users do NOT care about - they just

    want a device that's correct in footprint. And since footprints for

    connectors do NOT have any predefined name that is used all over the

    world, the user doesn't even know what to search for.

     

    And still worse: If, after years of searching, you DO find the right

    device, you might also find (after building the board, which didn't

    work) that there is some error in the library.

     

    Therefore: Whatever CAD program you're using, the FIRST thing you should

    learn is how to create your own libraries. Only in the most dire

    circumstances we use other people's libraries here. I myself spend just

    below 10% of my time creating EAGLE parts (but that's for about 20

    users). Of course that's all a lot of work, but it's the only

    possibility to get what YOU can work with easily. And, in the end,

    creating a part is often NOT more work than searching hours for the

    correct library device.

     

    A generic library with several hundred components and their packages

    > is by far much better.

     

    Yes. And since everybody has DIFFERENT library needs, everybody (or at

    least the EAGLE administrator) should build their own libraries.

     

    It should take minutes to build a package with any size pad,

    > number of pads and pitch without having to constantly change grid size

    > or copy pads to complete a high pad count package.

     

    Creating most through-hole devices DOES only take minutes, but for SMDs

    with their strange pad positions, which often do not even use the same

    grid in both directions, this is NOT nice. But here, the culprit is not

    EAGLE, but the component manufacturers, who think up designs that just

    ARE very complicated.

     

    True, EAGLE's library capabilities COULD be improved. There might even

    now exist some ULPs that help you in this respect, but I don't know

    them, and they're not available in the GUI, so new users will never find

    that functionality. But overall, I have the impression that only about

    30% of the library problems are CadSoft's, the other 70% are different

    user desires, strange manufacturer's designs,...

     

    Andreas Weidner