Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) UI - Mouse wheel middle click zooms and pans
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 188 subscribers
  • Views 2685 views
  • Users 0 members are here
  • ui
Related

UI - Mouse wheel middle click zooms and pans

helloworld922
helloworld922 over 14 years ago

I'm having some trouble with panning the UI. The issue is that whenever I click the middle button to pan, it also zooms in. If I hold the middle button down steady, it will continue to zoom in. This makes navigating through a schematic a huge pain. The only way I found to get around this is to change the mouse wheel zoom to 1 or 0, however both of these options eliminate zooming by scrolling the mouse wheel. I have the default 6.2.0 install for Windows.

 

Is there a way I can fix this so that I can pan with the middle button without the annoying zoom in and still be able to zoom by scrolling the mouse wheel?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    I have the same problem. But I also checked this with eagle5.

    eagle5 ignores if I tilt the wheel itself, so I can pan by pressing the

    wheel, and zoom by turning the wheel. the tilt is just ignored.

     

    Is there a setting where we can make eagle ignore this tilit?

     

    BR

    Marc

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    On 8/1/2012 10:22 AM, Marc Wetzel wrote:

    I have the same problem. But I also checked this with eagle5.

    eagle5 ignores if I tilt the wheel itself, so I can pan by pressing the

    wheel, and zoom by turning the wheel. the tilt is just ignored.

     

    Is there a setting where we can make eagle ignore this tilit?

     

    BR

    Marc

     

    Hi Marc,

     

    I hope you are doing well. You have to disable it in your OS's mouse

    properties. EAGLE uses whatever the OS will give it.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Jorge

     

    I think you are misssing that this behavior is new in V6.  No mouse settings were changed during the upgrade.

     

    There are no settings, at least in the control panel of Windows 7, that will affect this.

     

    In Eagle, setting the mouse wheel zoom to 0 allows the mouse to work normally - that is, spinning the wheel scrolls vertically, while pressing the wheel side to side does horizontal scrolling, but there is no zooming capability with this setting.  However, holding the wheel button down now causes the display to scroll from side to side while simultaneously panning.

     

    Setting the mouse wheel zoom to 1 eliminates all scrolling with the wheel, but panning works correctly.

     

    Setting the mouse wheel to the default 1.2 brings back the behavior of zooming when the wheel is held down (or pushed side to side).

     

    A lot of folks seem to be reporting the same problem.  It is Eagle V6 related, NOT an OS issue. 

     

    Thanks

    Bruce Herrick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    My Logitech M505 wireless mouse works exactly perfect with respect to scroll up=Zoom in, scroll down=Zoom out, right tilt=pan right, left tilt=pan left. That is except for Eagle 6.6. Works with all my browsers, every microsoft product, everything I have ever tried. Except Eagle. I doubt it is an OS issue. Just my 2 cents.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to autodeskguest

    I realize this is an old thread but I just updated from version 5 to version 7 and now I have this problem too, very frustrating.  Windows (7) will not allow me to turn the side-to-side control off; '1' is the lowest sensitivity setting instead of '0'.  This reduces the error but still makes the mouse frustrating to use for panning.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to autodeskguest

    Hi Jorge

     

    I am currently using an old mouse that does not have side-to-side capability, and it seems to work correctly.  I would prefer my cordless but this old one at least lets me get my work done.

     

    The other mouse does not zoom with a setting of 0.  Instead, when you press the button down it scrolls from side to side.  Rotating the wheel scrolls vertically as it should. 

     

    My OS is Windows 7 Professional 64 bit.

     

    Thanks for looking into this.

     

    Bruce Herrick

    10 year Eagle user

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 13 years ago in reply to e14 Contributor

    On 5/25/2013 4:39 PM, Bruce Herrick wrote:

    Jorge

     

    I think you are misssing that this behavior is new in V6.  No mouse

    settings were changed during the upgrade.

     

    There are no settings, at least in the control panel of Windows 7, that

    will affect this.

     

    In Eagle, setting the mouse wheel zoom to 0 allows the mouse to work

    normally - that is, spinning the wheel scrolls vertically, while

    pressing the wheel side to side does horizontal scrolling, but there is

    no zooming capability with this setting.  However, holding the wheel

    button down now causes the display to scroll from side to side while

    simultaneously panning.

     

    Setting the mouse wheel zoom to 1 eliminates all scrolling with the

    wheel, but panning works correctly.

     

    Setting the mouse wheel to the default 1.2 brings back the behavior of

    zooming when the wheel is held down (or pushed side to side).

     

    A lot of folks seem to be reporting the same problem.  It is Eagle V6

    related, NOT an OS issue.

     

    Thanks

    Bruce Herrick

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/77709#77709

     

     

    Hi Bruce,

     

    This is not entirely correct Bruce. V5 did not have any provisions to

    accept side to side input on a scroll wheel. The updated libraries that

    were used to compile V6 can accept this input and do something with it,

    but again it just taking what the OS will give it. Had V5 had support

    for the side-side tilt we would've started running into this in V5.

     

    The Mouse wheel zoom is simply a factor that control how much a turn of

    the scroll wheel zooms into the design. A value of zero disables the

    zooming functionality by turning the scroll wheel, so I don't see how it

    would still zoom after setting it to zero.

     

    To those experiencing this issue, do you have any other mice you can

    try? Preferrably scroll-wheel mice that don't support side-side tilt on

    the scroll wheel.

     

    Let me know what you guys can find out. If problems continue I'm going

    to need some way of reproducing the issue. Please specify the OS and

    whether it's 32-bit or 64-bit.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 13 years ago in reply to e14 Contributor

    On 5/25/2013 4:39 PM, Bruce Herrick wrote:

    Jorge

     

    I think you are misssing that this behavior is new in V6.  No mouse

    settings were changed during the upgrade.

     

    There are no settings, at least in the control panel of Windows 7, that

    will affect this.

     

    In Eagle, setting the mouse wheel zoom to 0 allows the mouse to work

    normally - that is, spinning the wheel scrolls vertically, while

    pressing the wheel side to side does horizontal scrolling, but there is

    no zooming capability with this setting.  However, holding the wheel

    button down now causes the display to scroll from side to side while

    simultaneously panning.

     

    Setting the mouse wheel zoom to 1 eliminates all scrolling with the

    wheel, but panning works correctly.

     

    Setting the mouse wheel to the default 1.2 brings back the behavior of

    zooming when the wheel is held down (or pushed side to side).

     

    A lot of folks seem to be reporting the same problem.  It is Eagle V6

    related, NOT an OS issue.

     

    Thanks

    Bruce Herrick

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/77709#77709

     

     

    Hi Bruce,

     

    This is not entirely correct Bruce. V5 did not have any provisions to

    accept side to side input on a scroll wheel. The updated libraries that

    were used to compile V6 can accept this input and do something with it,

    but again it just taking what the OS will give it. Had V5 had support

    for the side-side tilt we would've started running into this in V5.

     

    The Mouse wheel zoom is simply a factor that control how much a turn of

    the scroll wheel zooms into the design. A value of zero disables the

    zooming functionality by turning the scroll wheel, so I don't see how it

    would still zoom after setting it to zero.

     

    To those experiencing this issue, do you have any other mice you can

    try? Preferrably scroll-wheel mice that don't support side-side tilt on

    the scroll wheel.

     

    Let me know what you guys can find out. If problems continue I'm going

    to need some way of reproducing the issue. Please specify the OS and

    whether it's 32-bit or 64-bit.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    My Logitech M505 wireless mouse works exactly perfect with respect to scroll up=Zoom in, scroll down=Zoom out, right tilt=pan right, left tilt=pan left. That is except for Eagle 6.6. Works with all my browsers, every microsoft product, everything I have ever tried. Except Eagle. I doubt it is an OS issue. Just my 2 cents.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to autodeskguest

    I realize this is an old thread but I just updated from version 5 to version 7 and now I have this problem too, very frustrating.  Windows (7) will not allow me to turn the side-to-side control off; '1' is the lowest sensitivity setting instead of '0'.  This reduces the error but still makes the mouse frustrating to use for panning.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to autodeskguest

    Hi Jorge

     

    I am currently using an old mouse that does not have side-to-side capability, and it seems to work correctly.  I would prefer my cordless but this old one at least lets me get my work done.

     

    The other mouse does not zoom with a setting of 0.  Instead, when you press the button down it scrolls from side to side.  Rotating the wheel scrolls vertically as it should. 

     

    My OS is Windows 7 Professional 64 bit.

     

    Thanks for looking into this.

     

    Bruce Herrick

    10 year Eagle user