Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) UI - Mouse wheel middle click zooms and pans
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 188 subscribers
  • Views 2683 views
  • Users 0 members are here
  • ui
Related

UI - Mouse wheel middle click zooms and pans

helloworld922
helloworld922 over 14 years ago

I'm having some trouble with panning the UI. The issue is that whenever I click the middle button to pan, it also zooms in. If I hold the middle button down steady, it will continue to zoom in. This makes navigating through a schematic a huge pain. The only way I found to get around this is to change the mouse wheel zoom to 1 or 0, however both of these options eliminate zooming by scrolling the mouse wheel. I have the default 6.2.0 install for Windows.

 

Is there a way I can fix this so that I can pan with the middle button without the annoying zoom in and still be able to zoom by scrolling the mouse wheel?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    I have the same problem. But I also checked this with eagle5.

    eagle5 ignores if I tilt the wheel itself, so I can pan by pressing the

    wheel, and zoom by turning the wheel. the tilt is just ignored.

     

    Is there a setting where we can make eagle ignore this tilit?

     

    BR

    Marc

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    On 8/1/2012 10:22 AM, Marc Wetzel wrote:

    I have the same problem. But I also checked this with eagle5.

    eagle5 ignores if I tilt the wheel itself, so I can pan by pressing the

    wheel, and zoom by turning the wheel. the tilt is just ignored.

     

    Is there a setting where we can make eagle ignore this tilit?

     

    BR

    Marc

     

    Hi Marc,

     

    I hope you are doing well. You have to disable it in your OS's mouse

    properties. EAGLE uses whatever the OS will give it.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Jorge

     

    I think you are misssing that this behavior is new in V6.  No mouse settings were changed during the upgrade.

     

    There are no settings, at least in the control panel of Windows 7, that will affect this.

     

    In Eagle, setting the mouse wheel zoom to 0 allows the mouse to work normally - that is, spinning the wheel scrolls vertically, while pressing the wheel side to side does horizontal scrolling, but there is no zooming capability with this setting.  However, holding the wheel button down now causes the display to scroll from side to side while simultaneously panning.

     

    Setting the mouse wheel zoom to 1 eliminates all scrolling with the wheel, but panning works correctly.

     

    Setting the mouse wheel to the default 1.2 brings back the behavior of zooming when the wheel is held down (or pushed side to side).

     

    A lot of folks seem to be reporting the same problem.  It is Eagle V6 related, NOT an OS issue. 

     

    Thanks

    Bruce Herrick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    My Logitech M505 wireless mouse works exactly perfect with respect to scroll up=Zoom in, scroll down=Zoom out, right tilt=pan right, left tilt=pan left. That is except for Eagle 6.6. Works with all my browsers, every microsoft product, everything I have ever tried. Except Eagle. I doubt it is an OS issue. Just my 2 cents.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to autodeskguest

    I realize this is an old thread but I just updated from version 5 to version 7 and now I have this problem too, very frustrating.  Windows (7) will not allow me to turn the side-to-side control off; '1' is the lowest sensitivity setting instead of '0'.  This reduces the error but still makes the mouse frustrating to use for panning.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to autodeskguest

    I realize this is an old thread but I just updated from version 5 to version 7 and now I have this problem too, very frustrating.  Windows (7) will not allow me to turn the side-to-side control off; '1' is the lowest sensitivity setting instead of '0'.  This reduces the error but still makes the mouse frustrating to use for panning.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    My Logitech M505 wireless mouse works exactly perfect with respect to scroll up=Zoom in, scroll down=Zoom out, right tilt=pan right, left tilt=pan left. That is except for Eagle 6.6. Works with all my browsers, every microsoft product, everything I have ever tried. Except Eagle. I doubt it is an OS issue. Just my 2 cents.