I've found Sparkfun files for 6.0+ but when I tried to use them in Eagle 6.2 I get a message about
"Loading D:/Documents/SparkFun-Boards.lbr ...
Error:
line 5, column 6: This is not an EAGLE file." Anyone have updated files for Eagle 6.2?
I've found Sparkfun files for 6.0+ but when I tried to use them in Eagle 6.2 I get a message about
"Loading D:/Documents/SparkFun-Boards.lbr ...
Error:
line 5, column 6: This is not an EAGLE file." Anyone have updated files for Eagle 6.2?
Richard Waterman wrote:
I've found Sparkfun files for 6.0+ but when I tried to use them in
Eagle 6.2 I get a message about
"Loading D:/Documents/SparkFun-Boards.lbr ...
Error:
line 5, column 6: This is not an EAGLE file." Anyone have updated
files for Eagle 6.2?
Open up that Sparkfun library with a text editor and view the XML
There is a line near the top that looks similar to the following
sparkfun/SparkFun-Eagle-Libraries · GitHub
It has two starnge charcters in it. One after master and the other before
GitHub. These may be causing the issue so take them out and try again
HTH
Warren
--
Viewed / responded via the newsgroup at
news.cadsoft.de
Hi,
Thanks for giving that to try but didn't help. I wonder what version sparkfun actually uses to allow it to work. Maybe they stayed on 6.0.
Hi,
Thanks for giving that to try but didn't help. I wonder what version sparkfun actually uses to allow it to work. Maybe they stayed on 6.0.
Well that seemed to do it. Guess I did download them some wrong way before. Thanks alot now able to use em.
Am 10.09.2012 04:06, schrieb Richard Waterman:
Hi,
Thanks for giving that to try but didn't help. I wonder what version sparkfun actually uses to allow it to work. Maybe they stayed on 6.0.
https://github.com/sparkfun/SparkFun-Eagle-Libraries/downloads
Here is a link for eagle6 sparkfun libraries at github.
Maybe you downloaded the files directly and that won't work.
A little above the list at the very right side you can see
" Tags Download". Klick on download and you are given the choice to
download as zip/tar.gz file. After decompression the files are ready to
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
I seem to be able to load them just fine in 6.2