I'm new to using Eagle. I want to have some holes in my circuit board that I will solder wires into. How do I show these holes in the schematic? Is there a component that can represent this hole?
I'm new to using Eagle. I want to have some holes in my circuit board that I will solder wires into. How do I show these holes in the schematic? Is there a component that can represent this hole?
Hello Scott,
There's a standard library with Eagle for that: wirepad.lbr. Contains a
simple schematic simple and just one pad for the board, in different sizes.
Richard
Op Sun, 05 Aug 2012 00:15:36 +0200 schreef scott216
<noreply-119233@element14.com>:
I'm new to using Eagle. I want to have some holes in my circuit board
that I will solder wires into. How do I show these holes in the
schematic? Is there a component that can represent this hole?
If you want the connection points shown in the schematic, then ADD a
Hole component (with an assigned PAD). See holes.lbr for examples. The
Package can consist of just a Round PAD with a typical Drill size 0.033"
and Diameter 0.063" for AWG 22 wire. In a last-minute pinch, you could
always just add VIAs to the board, but you would lose desired documentation.
We also usually place a strain-relief hole next to the pads to run the
wire through to minimize strain on the solder point; you can just add
HOLEs in the Board design (large enough for the wire insulation).
On 8/4/2012 3:15 PM, scott216 wrote:
I'm new to using Eagle. I want to have some holes in my circuit board that I will solder wires into. How do I show these holes in the schematic? Is there a component that can represent this hole?