EAGLE User Support (English) How to add connection points for soldered wires
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 4208 views
  • Users 0 members are here
Related

How to add connection points for soldered wires

scott216
scott216 over 13 years ago

I'm new to using Eagle.  I want to have some holes in my circuit board that I will solder wires into.  How do I show these holes in the schematic? Is there a component that can represent this hole?

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 13 years ago

    If you want the connection points shown in the schematic, then ADD a

    Hole component (with an assigned PAD).  See holes.lbr for examples. The

    Package can consist of just a Round PAD with a typical Drill size 0.033"

    and Diameter 0.063" for AWG 22 wire.  In a last-minute pinch, you could

    always just add VIAs to the board, but you would lose desired documentation.

     

    We also usually place a strain-relief hole next to the pads to run the

    wire through to minimize strain on the solder point; you can just add

    HOLEs in the Board design (large enough for the wire insulation).

     

    On 8/4/2012 3:15 PM, scott216 wrote:

    I'm new to using Eagle.  I want to have some holes in my circuit board that I will solder wires into.  How do I show these holes in the schematic? Is there a component that can represent this hole?

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 13 years ago

    If you want the connection points shown in the schematic, then ADD a

    Hole component (with an assigned PAD).  See holes.lbr for examples. The

    Package can consist of just a Round PAD with a typical Drill size 0.033"

    and Diameter 0.063" for AWG 22 wire.  In a last-minute pinch, you could

    always just add VIAs to the board, but you would lose desired documentation.

     

    We also usually place a strain-relief hole next to the pads to run the

    wire through to minimize strain on the solder point; you can just add

    HOLEs in the Board design (large enough for the wire insulation).

     

    On 8/4/2012 3:15 PM, scott216 wrote:

    I'm new to using Eagle.  I want to have some holes in my circuit board that I will solder wires into.  How do I show these holes in the schematic? Is there a component that can represent this hole?