I have created few .lbr files and they appear withe a little padlock on Eagle but I cannot see them with Windows 7 explorer and I cannot reopen them to modify them. How can I get rid of this padlock?
I have created few .lbr files and they appear withe a little padlock on Eagle but I cannot see them with Windows 7 explorer and I cannot reopen them to modify them. How can I get rid of this padlock?
If you can't see it in windoze explorer, either you are looking under the
wrong rock or the files are "hidden" and you don't have the option set in
folder options to show hidden files. By default, one of the first things I
do when I do a windoze install on any of my stuff is to uncheck the option
to hide extensions of known file types and show hidden files. I HATE being
"helped" -- see of one of those conditions applies here.
mikey
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
I have this identical problem and not only the lbr file but its containing folder is hidden from File Explorer. The containing folder shows up in Eagle > Libraries with the padlock. The containing folder for the hidden folder, which is Eagle-6.2.0/lbr, has its permissions set to display hidden files and folders - so that is not the problem. What is going on here?
Well I finally gained access to the file. I had to go to Eagle Control Panel, select the file, Choose Copy from the context menu and then saved it on my Desktop. I still do not understand WTF is happening though. I changed permissions so that I would have Full Control from the Eagle folder on down and that did not help. I am perplexed. But at least if others run into this, there is a workaround through the Copy command.
<on soap box>
Another "invention" from the Bill Gates crowd! Duh, aren't some users smart enough to know better? You want to stop hackers
(maybe) stop giving "secret" interfaces. Ha Ha.
<off soap box>
Clem
Yeah, that is that "virtual store" issue I have been bitten by before. Microsoft has come up with this clever "scheme" whereby if you are not allowed to put something where you are trying to put it, then it puts it in the "virtual store" under your account and creates a link from where you thought you put it to where it is. Not a bad idea EXCEPT they don't tell you they did it and if you come at it from a different direction, you can't find the file. Do a bit of searching on the "virtual store" and you will have a better grasp of how it works (it has been a while since I managed to shoot myself in the foot with it). I first ran into it with the CCS C compiler when I tried to drag the license file from the CD they had sent me to the install folder where it was supposed to be. Kept getting a notice about "invalid license file". Had CCS send me a new file. Tried to drag that from the email to the install folder. Turns out both the email and the CD are considered "suspect" for lack of a better word by M$ and they do the "virtual store" thing with them then the compiler could not find the right one. The secret turned out to be to drag the file from the email to the desktop THEN drag it to the install folder and M$ decided that was safe enough I guess. I really hate being "hepped" - especially when it doesn't bother to tell you it did it. Either put the stupid file where I want it or tell me "permission denied" and let me work the problem, but don't put it somewhere else and tell me everything is OK !!!
Yeah, that is that "virtual store" issue I have been bitten by before. Microsoft has come up with this clever "scheme" whereby if you are not allowed to put something where you are trying to put it, then it puts it in the "virtual store" under your account and creates a link from where you thought you put it to where it is. Not a bad idea EXCEPT they don't tell you they did it and if you come at it from a different direction, you can't find the file. Do a bit of searching on the "virtual store" and you will have a better grasp of how it works (it has been a while since I managed to shoot myself in the foot with it). I first ran into it with the CCS C compiler when I tried to drag the license file from the CD they had sent me to the install folder where it was supposed to be. Kept getting a notice about "invalid license file". Had CCS send me a new file. Tried to drag that from the email to the install folder. Turns out both the email and the CD are considered "suspect" for lack of a better word by M$ and they do the "virtual store" thing with them then the compiler could not find the right one. The secret turned out to be to drag the file from the email to the desktop THEN drag it to the install folder and M$ decided that was safe enough I guess. I really hate being "hepped" - especially when it doesn't bother to tell you it did it. Either put the stupid file where I want it or tell me "permission denied" and let me work the problem, but don't put it somewhere else and tell me everything is OK !!!
<on soap box>
Another "invention" from the Bill Gates crowd! Duh, aren't some users smart enough to know better? You want to stop hackers
(maybe) stop giving "secret" interfaces. Ha Ha.
<off soap box>
Clem