I have created few .lbr files and they appear withe a little padlock on Eagle but I cannot see them with Windows 7 explorer and I cannot reopen them to modify them. How can I get rid of this padlock?
I have created few .lbr files and they appear withe a little padlock on Eagle but I cannot see them with Windows 7 explorer and I cannot reopen them to modify them. How can I get rid of this padlock?
If you can't see it in windoze explorer, either you are looking under the
wrong rock or the files are "hidden" and you don't have the option set in
folder options to show hidden files. By default, one of the first things I
do when I do a windoze install on any of my stuff is to uncheck the option
to hide extensions of known file types and show hidden files. I HATE being
"helped" -- see of one of those conditions applies here.
mikey
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
I have this identical problem and not only the lbr file but its containing folder is hidden from File Explorer. The containing folder shows up in Eagle > Libraries with the padlock. The containing folder for the hidden folder, which is Eagle-6.2.0/lbr, has its permissions set to display hidden files and folders - so that is not the problem. What is going on here?
Well I finally gained access to the file. I had to go to Eagle Control Panel, select the file, Choose Copy from the context menu and then saved it on my Desktop. I still do not understand WTF is happening though. I changed permissions so that I would have Full Control from the Eagle folder on down and that did not help. I am perplexed. But at least if others run into this, there is a workaround through the Copy command.
<on soap box>
Another "invention" from the Bill Gates crowd! Duh, aren't some users smart enough to know better? You want to stop hackers
(maybe) stop giving "secret" interfaces. Ha Ha.
<off soap box>
Clem
<on soap box>
Another "invention" from the Bill Gates crowd! Duh, aren't some users smart enough to know better? You want to stop hackers
(maybe) stop giving "secret" interfaces. Ha Ha.
<off soap box>
Clem