Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) route-bga.ulp
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 819 views
  • Users 0 members are here
  • eagle
  • route-bga
  • bga
Related

route-bga.ulp

SpacedCowboy
SpacedCowboy over 13 years ago

Does this ULP (Eagle 6.2 on a Mac) require the board to be configured for buried/blind vias ?

 

Whenever I run it, all that happens is that a dog-bone via is created and the signal is then routed out directly to the nearest edge. This works fine when there's no via in the way (from a closer-to-the-edge ball) but if there are multiple rows that need vias, it's completely useless.

 

Here's a picture of one such routed chip:

image

 

Ignoring that it failed to take into account the caps on the bottom side of the board, which I could live with, just running a DRC immediately after the "run route-bga U$1" command gives me 638 errors - there were 0 unapproved before the 'run...' command. Here's a close-up of what one part of the chip looks like:

 

image

I don't know what the problem is at D24,E24,... but clearly the problem for the via inside the {E22,E23,F22,F23} box is that it has E21 being routed *through* the via created for E22 to route out with. As far as I know, the only way that could work would be if the vias were generally expected to be blind.

 

Is this really the case ? I was hoping it would do a mini-autorouter kind of thing and find a way out for each via. This is a six-layer board, and given the "tracks" into the center formed by Vio/Vcc/Vdd I think it ought to be possible without blind vias. It's just damn annoying to keep on ripping up and retrying manually...

 

Simon

 

[ps: I can't get past the first page of the discussion, it just keeps saying "loading...", so apologies if this has been asked/answered before. There's no obvious discussion-specific search, either.]

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Simon Gornall wrote:

     

    .............................

    [ps: I can't get past the first page of the discussion, it just keeps

    saying "loading...", so apologies if this has been asked/answered

    before. There's no obvious discussion-specific search, either.]

    .........................

     

     

    Some of your query was answered earlier so seeing the full post is

    important.

    You are posting at Element14. There are real issues with that web portal

    into the CadSoft newsgroup and Element14 does not pass your images through

    so most of the'knowledge' does not see them unless they go and do battle

    with  the Element14 site, if they are curious about your image.

    Try the far better web portal at http://www.eaglecentral.ca/forums/

    To be able to post there you need to register and wait a couple of days for

    approval.(just a formality that is worth the wait)

     

    Or set up a newsreader for news.cadsoft.de

    That is the repository for all the posts. ie that one both web portals refer

    to.

     

    HTH

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • SpacedCowboy
    0 SpacedCowboy over 13 years ago in reply to e14 Contributor

    Ok - thanks. I thought Element14 and Cadsoft were supposed to be working hand-in-hand these days ... Ah well.

     

    If anyone is interested, and doesn't want to fight through the Element14 website, the images can be found at http://0x0000ff.com/imgs/eagle/bga-overview.png and http://0x0000ff.com/imgs/eagle/bga-closeup.png respectively, if that helps image

     

    Cheers

       Simon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • SpacedCowboy
    0 SpacedCowboy over 13 years ago in reply to e14 Contributor

    Ok - thanks. I thought Element14 and Cadsoft were supposed to be working hand-in-hand these days ... Ah well.

     

    If anyone is interested, and doesn't want to fight through the Element14 website, the images can be found at http://0x0000ff.com/imgs/eagle/bga-overview.png and http://0x0000ff.com/imgs/eagle/bga-closeup.png respectively, if that helps image

     

    Cheers

       Simon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to SpacedCowboy

    This ULP is pretty much garbage. I've been trying to use it for quite a while and I'm getting similar behavior. I'll be watching this thread to see if anyone can help you. Also, I'll let you know if I figure it out.