Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Ref-Package Library Not showing up
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 816 views
  • Users 0 members are here
Related

Ref-Package Library Not showing up

e14 Contributor
e14 Contributor over 13 years ago

I have been trying to get my eagle 6.2 and 6.1 to show the Ref-Packages in my add window in a schematic.  I have double checked the control panel and the ref packages are turned on and set to use.  What is the deal, why can't I get these to show up in my add window in the schematic.  I have tried to also reinstall but with no luck.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    On 9/17/2012 3:02 PM, Justin Man wrote:

    I have been trying to get my eagle 6.2 and 6.1 to show the Ref-Packages in my add window in a schematic.  I have double checked the control panel and the ref packages are turned on and set to use.  What is the deal, why can't I get these to show up in my add window in the schematic.  I have tried to also reinstall but with no luck.

     

     

    Hi Justin,

     

    Packages can't be placed in the schematic, hence why the ref-packages

    library doesn't show up in the schematic editor.

     

    If you use the add command in the board editor you will be able to see

    the ref-packages library.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Ah ha I see that now.  I have never used add in a way that you would add the part in the schematic.  When ever I try to add these now it says I can't backnotate.  So can I not integrate these with already created schematic?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Ah ha I see that now.  I have never used add in a way that you would add the part in the schematic.  When ever I try to add these now it says I can't backnotate.  So can I not integrate these with already created schematic?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    On 9/17/2012 5:40 PM, Justin Man wrote:

    Ah ha I see that now.  I have never used add in a way that you would add the part in the schematic.  When ever I try to add these now it says I can't backnotate.  So can I not integrate these with already created schematic?

     

     

    Hi Justin,

     

    You're partially correct. EAGLE won't allow you to bring in a package

    into the board because that would break consistency. It makes sense if

    you think about it, how many components in the world use a DIP-08

    package for instance? The LM741, LM555, TL082, etc. If you just bring

    the package into the layout how would the schematic reflect the specific

    part you're trying to use?

     

    The correct workflow is to setup everything in the schematic first that

    way things are setup for the board.

     

    What you should do is make a proper library components with associated

    symbol and package, put that in your schematic and then the package will

    follow. See Chp8 of the EAGLE manual for the most comprehensive tutorial

    or Google EAGLE tutorials you'll find several good ones. Dangerous

    Prototypes has a nice tutorial on library creation check it out.

     

    Best Regards,

    Jorge Garcia