Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Autorouter math- space for tracks between pads
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 187 subscribers
  • Views 356 views
  • Users 0 members are here
  • pad
  • pcb_traces
  • autorouter
Related

Autorouter math- space for tracks between pads

e14 Contributor
e14 Contributor over 13 years ago

I am trying to autoroute a fairly simple board with V5.11.0 after a long period of not using Eagle. I want to coerce the autorouter into

putting 8 mil tracks between the pins of a 2 mm through hole connector (87758-3416, from con-molex.lbr). I have reduced the connector

pad size in the library part from .050 to .045 in. diameter to allow more room. The math says: pads on 2mm centers=.07874 inch center-to-center.

With .045 pads that should allow .03374 free space between pads. With an 8 mil track there should be almost 13 mils space between the

track and pads. However I have to set the minimum space value to 6 mils (DRC->Clearance) for the router to run tracks between the pads.

This is too fine for the board prototype house (and good practice) and I don't see why the default value of 8 mils would not work when there is 12.87 mils of

space- if I set this value to 8 mils I get DRC clearance violations. Placement and routing grids are set at .001. Any suggestions would be appreciated!

Thanks

Harry

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 13 years ago

    Harry Sieber wrote:

    I am trying to autoroute a fairly simple board with V5.11.0 after a

    long period of not using Eagle. I want to coerce the autorouter into

    putting 8 mil tracks between the pins of a 2 mm through hole

    connector (87758-3416, from con-molex.lbr). I have reduced the

    connector

    pad size in the library part from .050 to .045 in. diameter to allow

    more room. The math says: pads on 2mm centers=.07874 inch

    center-to-center.

    With .045 pads that should allow .03374 free space between pads. With

    an 8 mil track there should be almost 13 mils space between the

    track and pads. However I have to set the minimum space value to 6

    mils (DRC->Clearance) for the router to run tracks between the pads.

    This is too fine for the board prototype house (and good practice)

    and I don't see why the default value of 8 mils would not work when

    there is 12.87 mils of space- if I set this value to 8 mils I get DRC

    clearance violations. Placement and routing grids are set at .001.

    Any suggestions would be appreciated! Thanks

    Harry

     

     

     

     

    Looking at the library, and not changing the pad diameter, it appears that

    it should all work for you.

    BUT!...Measure the pad diameters and space between them on the board.

     

    Its likely the DRC settings have increased the size of the pads on the board

    and thus narrowed the gap. You reduced the pad diameter in the library but

    the diameter they end up as on the board is related to a percentage of the

    drill diameter.

    The library, for all intents and purposes, can really only force pads larger

    than what the DRC will calculate.

     

    The restring as measured in the library is 7mil but likley your DRC setting

    is 10mil so they increases to 10mil. While in the library if you make the

    pad diameter AUTO it will be depicted with a size determined by the DRC

    settings (based on the drill diameter) Making the minimum setting 9mil in

    the DRC enables an 8mil wire to pass though with 8mil clearances. Be aware

    though that all pads will be reduced to 9mil restrings if the maths

    calculates a size smaller than 9mil initially.

     

     

    HTH

    Warren

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 13 years ago

    On Mon, 24 Sep 2012 13:05:25 +0000, Harry Sieber wrote:

     

    I am trying to autoroute a fairly simple board with V5.11.0 after a long

    period of not using Eagle. I want to coerce the autorouter into putting

    8 mil tracks between the pins of a 2 mm through hole connector

    (87758-3416, from con-molex.lbr). I have reduced the connector pad size

    in the library part from .050 to .045 in. diameter to allow more room.

    The math says: pads on 2mm centers=.07874 inch center-to-center.

    With .045 pads that should allow .03374 free space between pads. With an

    8 mil track there should be almost 13 mils space between the track and

    pads. However I have to set the minimum space value to 6 mils

    (DRC->Clearance) for the router to run tracks between the pads.

    This is too fine for the board prototype house (and good practice) and I

    don't see why the default value of 8 mils would not work when there is

    12.87 mils of space- if I set this value to 8 mils I get DRC clearance

    violations. Placement and routing grids are set at .001. Any suggestions

    would be appreciated! Thanks Harry

     

    I've had similar problems.

     

    Place everything on a metric grid (use control-click to pick parts up by

    their centers, so when you put them down they'll be on-grid).  Then route

    on a metric grid.

     

    It's a pain in the behind if you've already got everything placed on an

    inch grid, but if you have a preponderance of metric "problem parts" then

    that's the way to go.

     

    I couldn't tell you what to do if you had a mix of metric and English

    fine-pitch parts, though.

     

    --

    Tim Wescott

    Control system and signal processing consulting

    www.wescottdesign.com