Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Autorouter math- space for tracks between pads
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 187 subscribers
  • Views 358 views
  • Users 0 members are here
  • pad
  • pcb_traces
  • autorouter
Related

Autorouter math- space for tracks between pads

e14 Contributor
e14 Contributor over 13 years ago

I am trying to autoroute a fairly simple board with V5.11.0 after a long period of not using Eagle. I want to coerce the autorouter into

putting 8 mil tracks between the pins of a 2 mm through hole connector (87758-3416, from con-molex.lbr). I have reduced the connector

pad size in the library part from .050 to .045 in. diameter to allow more room. The math says: pads on 2mm centers=.07874 inch center-to-center.

With .045 pads that should allow .03374 free space between pads. With an 8 mil track there should be almost 13 mils space between the

track and pads. However I have to set the minimum space value to 6 mils (DRC->Clearance) for the router to run tracks between the pads.

This is too fine for the board prototype house (and good practice) and I don't see why the default value of 8 mils would not work when there is 12.87 mils of

space- if I set this value to 8 mils I get DRC clearance violations. Placement and routing grids are set at .001. Any suggestions would be appreciated!

Thanks

Harry

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 13 years ago

    On Mon, 24 Sep 2012 13:05:25 +0000, Harry Sieber wrote:

     

    I am trying to autoroute a fairly simple board with V5.11.0 after a long

    period of not using Eagle. I want to coerce the autorouter into putting

    8 mil tracks between the pins of a 2 mm through hole connector

    (87758-3416, from con-molex.lbr). I have reduced the connector pad size

    in the library part from .050 to .045 in. diameter to allow more room.

    The math says: pads on 2mm centers=.07874 inch center-to-center.

    With .045 pads that should allow .03374 free space between pads. With an

    8 mil track there should be almost 13 mils space between the track and

    pads. However I have to set the minimum space value to 6 mils

    (DRC->Clearance) for the router to run tracks between the pads.

    This is too fine for the board prototype house (and good practice) and I

    don't see why the default value of 8 mils would not work when there is

    12.87 mils of space- if I set this value to 8 mils I get DRC clearance

    violations. Placement and routing grids are set at .001. Any suggestions

    would be appreciated! Thanks Harry

     

    I've had similar problems.

     

    Place everything on a metric grid (use control-click to pick parts up by

    their centers, so when you put them down they'll be on-grid).  Then route

    on a metric grid.

     

    It's a pain in the behind if you've already got everything placed on an

    inch grid, but if you have a preponderance of metric "problem parts" then

    that's the way to go.

     

    I couldn't tell you what to do if you had a mix of metric and English

    fine-pitch parts, though.

     

    --

    Tim Wescott

    Control system and signal processing consulting

    www.wescottdesign.com

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 13 years ago

    On Mon, 24 Sep 2012 13:05:25 +0000, Harry Sieber wrote:

     

    I am trying to autoroute a fairly simple board with V5.11.0 after a long

    period of not using Eagle. I want to coerce the autorouter into putting

    8 mil tracks between the pins of a 2 mm through hole connector

    (87758-3416, from con-molex.lbr). I have reduced the connector pad size

    in the library part from .050 to .045 in. diameter to allow more room.

    The math says: pads on 2mm centers=.07874 inch center-to-center.

    With .045 pads that should allow .03374 free space between pads. With an

    8 mil track there should be almost 13 mils space between the track and

    pads. However I have to set the minimum space value to 6 mils

    (DRC->Clearance) for the router to run tracks between the pads.

    This is too fine for the board prototype house (and good practice) and I

    don't see why the default value of 8 mils would not work when there is

    12.87 mils of space- if I set this value to 8 mils I get DRC clearance

    violations. Placement and routing grids are set at .001. Any suggestions

    would be appreciated! Thanks Harry

     

    I've had similar problems.

     

    Place everything on a metric grid (use control-click to pick parts up by

    their centers, so when you put them down they'll be on-grid).  Then route

    on a metric grid.

     

    It's a pain in the behind if you've already got everything placed on an

    inch grid, but if you have a preponderance of metric "problem parts" then

    that's the way to go.

     

    I couldn't tell you what to do if you had a mix of metric and English

    fine-pitch parts, though.

     

    --

    Tim Wescott

    Control system and signal processing consulting

    www.wescottdesign.com