Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Device/symbol without a package..
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 162 views
  • Users 0 members are here
Related

Device/symbol without a package..

e14 Contributor
e14 Contributor over 13 years ago

All,

 

I have to do a wiring diagram for a pld system. I've made schematic symbols for CPU's, Relays, Circuit breakers, etc. etc. I created a device without a package and would like to add it to a schematic. It errors and says there's no package. Exactly like a Volage rail connection, or a ground connection. Why can't I do this??

 

Thanks,


Cam

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    On 08.10.2012 22:40, Cameron Sweet wrote:

    All,

     

    I have to do a wiring diagram for a pld system. I've made schematic symbols for CPU's, Relays, Circuit breakers, etc. etc. I created a device without a package and would like to add it to a schematic. It errors and says there's no package. Exactly like a Volage rail connection, or a ground connection. Why can't I do this??

     

    Thanks,

     

    Cam

     

     

    EAGLE always expects to have a symbol that is connected to a package.

    As soon as you are using a pin in the symbol you need a pad in the

    package. Can you draw the symbols without pins? Then you wouldn't need

    a package....

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    On 08.10.2012 22:40, Cameron Sweet wrote:

    All,

     

    I have to do a wiring diagram for a pld system. I've made schematic symbols for CPU's, Relays, Circuit breakers, etc. etc. I created a device without a package and would like to add it to a schematic. It errors and says there's no package. Exactly like a Volage rail connection, or a ground connection. Why can't I do this??

     

    Thanks,

     

    Cam

     

     

    EAGLE always expects to have a symbol that is connected to a package.

    As soon as you are using a pin in the symbol you need a pad in the

    package. Can you draw the symbols without pins? Then you wouldn't need

    a package....

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/