Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) PCB editor does not respond to mouse clicks
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 1179 views
  • Users 0 members are here
  • eagle
  • mouse
  • question
Related

PCB editor does not respond to mouse clicks

e14 Contributor
e14 Contributor over 13 years ago

all  of a sudden Eagle 6.3 (free version) does not respond to mouse clicks properly.  Sometimes I can click on an icon like the eyeball and I click on the pcb trace and it works - but most of the time it seems to be clicking the eyeball icon over and over no matter where I click on the pcb.  Mouse wheel seems to work as expected but sometimes when I wheel click to pan the drawing jumps to some other location before beginning the pan operation.  similar problems in schematic editor.  I uninstalled and reinstalled and that did not help.  In AutoCAD the mouse buttons work as expected as does mouse wheel for zoom and pan.  Other applications seem to work properly. 

 

Mouse - MS Wireless Mobile Mouse 3500

OS = XP Pro

Dell Precision M4400 with 4 GB memory

 

 

Any ideas on what the problem might be?

 

Thanks,

 

Burke

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I suggest you try with a wired mouse.

    If that fixes the problem then the batteries may need replacing/charging in

    your wireless mouse.

     

    All the best.

    Warren

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zainka
    0 zainka over 13 years ago in reply to e14 Contributor

    On 15. nov. 2012 19:13, Burke Mitchell wrote:

    I have been experimenting and found that the mouse clicks only work properly after switching from small window to full screen or vice versa as stated in my last post.  However, if I try to add part to the schematic I find that after picking the part from the library window and clicking OK the part appears on the schematic wherever my mouse happens to be at the time.  However, when I try to move the mouse and the part to the desired location it just stays where it originally appeared.  I thought I might be able to move it using the move command but when I expand and contract the window then click the move button, the part disappears.

     

    I have uninstalled and reinstalled 6.3 and 6.2 and neither works with my mouse.  I also tried to use the touch pad and that is actually worse.

     

    Help!!!!!

     

    Burke

     

     

    Hi

     

    Its a while since I used Windows after switching fully to Linux, but it

    comes to me that there is a eagle settings file in your user folder

    somewhere in documents and settings.

     

    Did you delete this after uninstalling Eagle? Chance is that the mouce

    button assignments are stored here and preserved after uninstalling

    eagle. A fresh installation will first check for its existence before

    eventually creating it thus inherit old settings.

     

    If this does not help, then you should also flush the register for any

    traces of eagle settings key.

     

     

     

    Breg

    Vidar (Z)

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I have been experimenting and found that the mouse clicks only work properly after switching from small window to full screen or vice versa as stated in my last post.  However, if I try to add part to the schematic I find that after picking the part from the library window and clicking OK the part appears on the schematic wherever my mouse happens to be at the time.  However, when I try to move the mouse and the part to the desired location it just stays where it originally appeared.  I thought I might be able to move it using the move command but when I expand and contract the window then click the move button, the part disappears.

     

    I have uninstalled and reinstalled 6.3 and 6.2 and neither works with my mouse.  I also tried to use the touch pad and that is actually worse.

     

    Help!!!!!

     

    Burke

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I re-checked the settings for the mouse buttons and they are as they were before when it all worked properly.  The left button is set as simply a click (as is the right button and the middle wheel/button).  It acts like the mouse is stuck over the user interface button I click when the program first opens.  When I click the eyeball the first time it goes to its depressed state.  When I move off the eyeball and click somewhere else I can see the eyeball button acting like I had clicked it again.  I can click on the menu or anywhere except the minimize, close and normal/full screen buttons and it acts the same.  Just now while testing to see if the the normal/full screen button worked I found that after clicking that button the mouse works for one click.  So I can change the action from the eyeball to the move button but can't move anything.  If I shrink then expand the window again a click will now perform the command indicated - so then I can move a componant.  If I shrink and expand the window after each mouse click I can get work done but it is obviously very slow and cumbersome.

     

    Thanks for your help,

     

    Burke

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    On 09.10.2012 23:26, Burke Mitchell wrote:

    all  of a sudden Eagle 6.3 (free version) does not respond to mouse clicks properly.  Sometimes I can click on an icon like the eyeball and I click on the pcb trace and it works - but most of the time it seems to be clicking the eyeball icon over and over no matter where I click on the pcb.  Mouse wheel seems to work as expected but sometimes when I wheel click to pan the drawing jumps to some other location before beginning the pan operation.  similar problems in schematic editor.  I uninstalled and reinstalled and that did not help.  In AutoCAD the mouse buttons work as expected as does mouse wheel for zoom and pan.  Other applications seem to work properly.

     

    Mouse - MS Wireless Mobile Mouse 3500

    OS = XP Pro

    Dell Precision M4400 with 4 GB memory

     

    >

    Any ideas on what the problem might be?

     

    Thanks,

     

    Burke

     

     

    Hi,

     

    could it be a matter of what is assigned to the left mouse button? Is

    it a simple mouse click or could it be a double click?

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/