Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) PCB editor does not respond to mouse clicks
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 1182 views
  • Users 0 members are here
  • eagle
  • mouse
  • question
Related

PCB editor does not respond to mouse clicks

e14 Contributor
e14 Contributor over 13 years ago

all  of a sudden Eagle 6.3 (free version) does not respond to mouse clicks properly.  Sometimes I can click on an icon like the eyeball and I click on the pcb trace and it works - but most of the time it seems to be clicking the eyeball icon over and over no matter where I click on the pcb.  Mouse wheel seems to work as expected but sometimes when I wheel click to pan the drawing jumps to some other location before beginning the pan operation.  similar problems in schematic editor.  I uninstalled and reinstalled and that did not help.  In AutoCAD the mouse buttons work as expected as does mouse wheel for zoom and pan.  Other applications seem to work properly. 

 

Mouse - MS Wireless Mobile Mouse 3500

OS = XP Pro

Dell Precision M4400 with 4 GB memory

 

 

Any ideas on what the problem might be?

 

Thanks,

 

Burke

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    On 09.10.2012 23:26, Burke Mitchell wrote:

    all  of a sudden Eagle 6.3 (free version) does not respond to mouse clicks properly.  Sometimes I can click on an icon like the eyeball and I click on the pcb trace and it works - but most of the time it seems to be clicking the eyeball icon over and over no matter where I click on the pcb.  Mouse wheel seems to work as expected but sometimes when I wheel click to pan the drawing jumps to some other location before beginning the pan operation.  similar problems in schematic editor.  I uninstalled and reinstalled and that did not help.  In AutoCAD the mouse buttons work as expected as does mouse wheel for zoom and pan.  Other applications seem to work properly.

     

    Mouse - MS Wireless Mobile Mouse 3500

    OS = XP Pro

    Dell Precision M4400 with 4 GB memory

     

    >

    Any ideas on what the problem might be?

     

    Thanks,

     

    Burke

     

     

    Hi,

     

    could it be a matter of what is assigned to the left mouse button? Is

    it a simple mouse click or could it be a double click?

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I re-checked the settings for the mouse buttons and they are as they were before when it all worked properly.  The left button is set as simply a click (as is the right button and the middle wheel/button).  It acts like the mouse is stuck over the user interface button I click when the program first opens.  When I click the eyeball the first time it goes to its depressed state.  When I move off the eyeball and click somewhere else I can see the eyeball button acting like I had clicked it again.  I can click on the menu or anywhere except the minimize, close and normal/full screen buttons and it acts the same.  Just now while testing to see if the the normal/full screen button worked I found that after clicking that button the mouse works for one click.  So I can change the action from the eyeball to the move button but can't move anything.  If I shrink then expand the window again a click will now perform the command indicated - so then I can move a componant.  If I shrink and expand the window after each mouse click I can get work done but it is obviously very slow and cumbersome.

     

    Thanks for your help,

     

    Burke

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I re-checked the settings for the mouse buttons and they are as they were before when it all worked properly.  The left button is set as simply a click (as is the right button and the middle wheel/button).  It acts like the mouse is stuck over the user interface button I click when the program first opens.  When I click the eyeball the first time it goes to its depressed state.  When I move off the eyeball and click somewhere else I can see the eyeball button acting like I had clicked it again.  I can click on the menu or anywhere except the minimize, close and normal/full screen buttons and it acts the same.  Just now while testing to see if the the normal/full screen button worked I found that after clicking that button the mouse works for one click.  So I can change the action from the eyeball to the move button but can't move anything.  If I shrink then expand the window again a click will now perform the command indicated - so then I can move a componant.  If I shrink and expand the window after each mouse click I can get work done but it is obviously very slow and cumbersome.

     

    Thanks for your help,

     

    Burke