Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Copying and Moving Nets to different pins. Not possible to be efficient?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 189 subscribers
  • Views 801 views
  • Users 0 members are here
  • eagle
  • schematic
  • question
Related

Copying and Moving Nets to different pins. Not possible to be efficient?

jdavelement
jdavelement over 13 years ago

A few things are slowing down my productivity now that I'm using Eagle.  I'm thinking someone knows some tricks to the biggest issues here:

 

I frequently change my mind on the pin assignment the nets to optimize layout to a CPU, BUT Eagle won't MOVE  connected nets or disconnect nets that are connected so that I can move them to a different pin.  I'd use COPY, but then they don't connect!  That's also a problem.  I used to just copy the net drawing to all the places it went.  It was a breeze.  Now I have to reenter the net for every component is goes to?  How do I get around this? 

 

If I have to redraw the net and re-type the names of all of my nets just to change the pin assignments I need to quit my job where they make me use Eagle.  It's driving me mad.  Please help save a job or my sanity! 

 

It's as if everything that took one-click in my old ProCAD software seems to take 3 in Eagle.  But I'm trying not to be a big whiner, I just want to go forward with supported software, so I trust that some scripts will get me efficient again.  (I've been doing layout for 15 years and have done a couple hundred different board designs, so I'm not a newbie.)

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Op Tue, 30 Oct 2012 08:55:41 +0100 schreef Joel Davel 

    <noreply-135898@element14.com>:

     

    A few things are slowing down my productivity now that I'm using Eagle.  

    I'm thinking someone knows some tricks to the biggest issues here:

     

    I frequently change my mind on the pin assignment the nets to optimize 

    layout to a CPU, BUT Eagle won't MOVE  connected nets or disconnect nets 

    that are connected so that I can move them to a different pin.  I'd use 

    COPY, but then they don't connect!  That's also a problem.  I used to 

    just copy the net drawing to all the places it went.  It was a breeze.  

    Now I have to reenter the net for every component is goes to?  How do I 

    get around this?

    If I have to redraw the net and re-type the names of all of my nets just 

    to change the pin assignments I need to quit my job where they make me 

    use Eagle.  It's driving me mad.  Please help save a job or my sanity!

    It's as if everything that took one-click in my old ProCAD software 

    seems to take 3 in Eagle.  But I'm trying not to be a big whiner, I just 

    want to go forward with supported software, so I trust that some scripts 

    will get me efficient again.  (I've been doing layout for 15 years and 

    have done a couple hundred different board designs, so I'm not a newbie.)

     

     

     

    Hello Joel,

     

    It could be that I don't understand exactly what you're asking, but isn't 

    PINSWAP what you're looking for?

     

    From the HELP:

     

    The PINSWAP command is used to swap pins within the same symbol which have 

    been allocated the same swaplevel (> 0). Swaplevel, see PIN command. If a 

    board is tied to a schematic via Back Annotation two pads can only be 

    swapped if the related pins are swappable.

    On a board without a schematic this command permits two pads in the same 

    package to be swapped. The Swaplevel is not checked in this case.

    Wires attached to the swapped pins are moved with the pins so that short 

    circuits may appear. Please perform the DRC and correct possible errors.

     

    HTH,

     

    Richard

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jdavelement
    0 jdavelement over 13 years ago

    OK.  I'm answering my own question.  So to disconnect I need to COPY the nets and delete the originals; and to reconnect I need to place the copied nets on the new pins (still unconnected) but then move the component to the nets rather than the other way around.  Well. . .
    one important issue dealt with, though I'm open to other solutions.

     

    Smaller issues:

     

    1) Measuring distances with "mark" doesn't measure the alternate grid distance even when "mark" is placed on the alternate grid.  Any more efficient way to measure small relative distances?  I wish there was mini version of the dimension tool

     

    2) LABEL need to be re-established everytime when copying single nets without grouping them.  Personally I think labels should default on (as if grouped) for custom named nets.  Otherwise you could get into trouble with net-name shorts.