Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) BUG in v 6.3.0 : nets don't always connect - animated GIF to demonstrate (Eagle v6.3.0 Pro)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 889 views
  • Users 0 members are here
  • net
  • editor
  • bug
  • schematic
Related

BUG in v 6.3.0 : nets don't always connect - animated GIF to demonstrate (Eagle v6.3.0 Pro)

e14 Contributor
e14 Contributor over 13 years ago

Hello CadSoft (and the community),

 

I believe I have found a bug in the schematic editor (version 6.3.0). Please see this animated gif which demonstrates a problem we have encountered with the schematic editor. Please note all items are perfectly on grid.

 

When moving a device onto an drawn net, the connection is made (CORRECT!)

- HOWEVER -

When moving a net onto a device, the connection is *not* made (BUG?)

 

I really hope somebody from CadSoft can't comment on this behavior - and whether it is intentional. We are not used to this - because other editors (eg. simulation software such as LTSpice) properly make the connection.

 

Thanks!

 

http://eagle-bug.s3.amazonaws.com/connection.gif

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    On 13/11/12 21:00, B Mac wrote:

    Hello CadSoft (and the community),

     

    I believe I have found a bug in the schematic editor (version 6.3.0). Please see this animated gif which demonstrates a problem we have encountered with the schematic editor. Please note all items are perfectly on grid.

     

    When moving a device onto an drawn net, the connection is made (CORRECT!)

    - HOWEVER -

    When moving a net onto a device, the connection is not made (BUG?)

     

     

    Not a bug. This is just how it has always been with Eagle. You get used

    to it fairly quickly.

     

    Cheers,

    Rob

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I just read about that recently - I thought it was in the V6 tutorial, but

    I can't find it now.  I do remember reading though that the operation was

    not symmetrical.

     

    mikey

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    OK, found the statement I was looking for - see page 38 of the version 6.3

    tutorial from Cadsoft - it says next to the "Move" Icon -

    "No electrical connection will be generated if you MOVE a net line over a

    pin.

    On the other hand: if you move a pin over another pin or over a net line,

    an

    electrical connection will be generated, and a net line will be attached to

    the

    pin when the component is moved further. Remember the UNDO command if

    you want to detach the net line."

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    OK, found the statement I was looking for - see page 38 of the version 6.3

    tutorial from Cadsoft - it says next to the "Move" Icon -

    "No electrical connection will be generated if you MOVE a net line over a

    pin.

    On the other hand: if you move a pin over another pin or over a net line,

    an

    electrical connection will be generated, and a net line will be attached to

    the

    pin when the component is moved further. Remember the UNDO command if

    you want to detach the net line."

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.