Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 6.3.0 on Xubuntu 12.10
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 189 subscribers
  • Views 559 views
  • Users 0 members are here
Related

Eagle 6.3.0 on Xubuntu 12.10

e14 Contributor
e14 Contributor over 13 years ago

I recently installed Eagle 6.3.0 (using the shell script on Cadsoft's Downloads page) on Xubuntu 12.10 and I'm seeing some problems when trying to draw a schematic or create a symbol, etc. Specifically, the "edit screen" doesn't seem to refresh correctly so I get some whited out areas and copied parts of the image. I've attached a screenshot to show what I mean.

 

Also note that I installed an older version of Eagle (5.12) through my package manager and the problem existed there as well. This, together with the fact that I have used Eagle on previous installations of Xubuntu (12.04) and have not had this issue leads me to believe that it is something on the Linux side. However, I asked on Xubuntu's IRC channel and another user of Eagle + Xubuntu 12.10 said they do not see the same issue.

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I forgot to mention that I am on a 64-bit release of Xubuntu 12.10. I've installed all of the lib32 libraries listed in the FAQ: Eagle and 64-bit Linux Systems. Has anyone had a problem like this? I've seen people mention having problems with the actual installation process, but I haven't had any issues with that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I forgot to mention that I am on a 64-bit release of Xubuntu 12.10. I've installed all of the lib32 libraries listed in the FAQ: Eagle and 64-bit Linux Systems. Has anyone had a problem like this? I've seen people mention having problems with the actual installation process, but I haven't had any issues with that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • uboard
    0 uboard over 13 years ago in reply to e14 Contributor

    Same here!

     

    First installed 5.12 from repositories, but had this redraw / refresh glitch. After installing 6.3.0 and running it straight away, it was fine, but next day booting my machine again, the problem now is there in 6.3.0 as well.

     

    Running Xubuntu 12.10 64bit on AMD cpu/gpu (using AMD's proprietary "fglrx-updates" video drivers from repositories - ).

    Disabling desktop compositing didn't help either.

    Setting video driver to open source "xserver-xorg-video-ati" solves glitches in Eagle 6.3.0, but causes other problems.