Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) PCB ground plane not connecting to ground pins
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 3806 views
  • Users 0 members are here
Related

PCB ground plane not connecting to ground pins

e14 Contributor
e14 Contributor over 13 years ago

Hello,

 

I did some PCBs with Eagle, so I was quite sure I know it's basics, especially when it comes to ground and power planes.

 

I have a LQFP-100 device with some pins supposed to be connected to ground. I made a ground plane on the top layer, named it GND, same name as the gound net on schematics. Yet the plygon won't connect to the gound pins. I've put right next to the LQFP a different device (USB port) with ground pins as well - those are connected just fine.

image

 

Big pad on the bottom right is the GND pad of the USB connector, as you can see an airwire is led to the LQFP pin. There are some "blobs" or whatever on both sides of the unconnected pin.

I think I've clicked just about everything in Eagle, still no-go.

 

Eagle 6.2.0 Light.

 

 

Regards

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    On Sun, 06 Jan 2013 13:08:22 +0000, Michal Lesiak wrote:

     

    Hello,

     

    I did some PCBs with Eagle, so I was quite sure I know it's basics,

    especially when it comes to ground and power planes.

     

    I have a LQFP-100 device with some pins supposed to be connected to

    ground. I made a ground plane on the top layer, named it GND, same name

    as the gound net on schematics. Yet the plygon won't connect to the

    gound pins. I've put right next to the LQFP a different device (USB

    port) with ground pins as well - those are connected just fine.

    Image:pcb-gndplane.PNG

     

    Big pad on the bottom right is the GND pad of the USB connector, as you

    can see an airwire is led to the LQFP pin. There are some "blobs" or

    whatever on both sides of the unconnected pin.

    I think I've clicked just about everything in Eagle, still no-go.

     

    Eagle 6.2.0 Light.

     

     

    Regards

     

    Check the trace size of the polygon that you're using to define the

    ground plane.  It may be that the polygon trace size is too large to make

    the connection to the package.

     

    --

    Tim Wescott

    Control system and signal processing consulting

    www.wescottdesign.com

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    On Sun, 06 Jan 2013 13:08:22 +0000, Michal Lesiak wrote:

     

    Hello,

     

    I did some PCBs with Eagle, so I was quite sure I know it's basics,

    especially when it comes to ground and power planes.

     

    I have a LQFP-100 device with some pins supposed to be connected to

    ground. I made a ground plane on the top layer, named it GND, same name

    as the gound net on schematics. Yet the plygon won't connect to the

    gound pins. I've put right next to the LQFP a different device (USB

    port) with ground pins as well - those are connected just fine.

    Image:pcb-gndplane.PNG

     

    Big pad on the bottom right is the GND pad of the USB connector, as you

    can see an airwire is led to the LQFP pin. There are some "blobs" or

    whatever on both sides of the unconnected pin.

    I think I've clicked just about everything in Eagle, still no-go.

     

    Eagle 6.2.0 Light.

     

     

    Regards

     

    Check the trace size of the polygon that you're using to define the

    ground plane.  It may be that the polygon trace size is too large to make

    the connection to the package.

     

    --

    Tim Wescott

    Control system and signal processing consulting

    www.wescottdesign.com

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer