Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) PCB ground plane not connecting to ground pins
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 3793 views
  • Users 0 members are here
Related

PCB ground plane not connecting to ground pins

e14 Contributor
e14 Contributor over 13 years ago

Hello,

 

I did some PCBs with Eagle, so I was quite sure I know it's basics, especially when it comes to ground and power planes.

 

I have a LQFP-100 device with some pins supposed to be connected to ground. I made a ground plane on the top layer, named it GND, same name as the gound net on schematics. Yet the plygon won't connect to the gound pins. I've put right next to the LQFP a different device (USB port) with ground pins as well - those are connected just fine.

image

 

Big pad on the bottom right is the GND pad of the USB connector, as you can see an airwire is led to the LQFP pin. There are some "blobs" or whatever on both sides of the unconnected pin.

I think I've clicked just about everything in Eagle, still no-go.

 

Eagle 6.2.0 Light.

 

 

Regards

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Be aware that it is not good practice to use zero width  polygon wires.

    That will make gerber files large. I tried your situation and could get it

    working with 7 mil wires with 8 mil spacing in the DRC.

     

    Warren

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Thank you all, indeed it was the problem with polygon trace widh - had to set it to 0 to make it work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    A side note,

     

    Your isolation seems to be really small. This is the gap between the GND flood and the other, non GND pins. Try setting it to around 10 or 12 mil, to prevent accidental shorts caused by manufacturing errors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    You can see the problem in the image with adjacent pins connected.

    Note the distance the polygon is keeping away from the other pins(signals)

    Now imagine that distance must be clear from a pin either side of a GND

    pin. That does not leave room for a very wide trace.

     

    So you need to balance.

    (1) The polygon wire width. This will be the width of the trace attempting

    to connect to the pin if it can without braking the required clearances

    rules.

     

    (2) The DRC and Class clearance rules governing how far signals must be

    away from other signals 

     

    (3) A grid that is fine enough so that the above clearances can still be

    satisfied if the pin/grid alignment is less than optimal

     

    (4) For Autorouting a routing grid that satisfies similarly to point (3)

     

     

    HTH

    Warren  

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    On Sun, 06 Jan 2013 13:08:22 +0000, Michal Lesiak wrote:

     

    Hello,

     

    I did some PCBs with Eagle, so I was quite sure I know it's basics,

    especially when it comes to ground and power planes.

     

    I have a LQFP-100 device with some pins supposed to be connected to

    ground. I made a ground plane on the top layer, named it GND, same name

    as the gound net on schematics. Yet the plygon won't connect to the

    gound pins. I've put right next to the LQFP a different device (USB

    port) with ground pins as well - those are connected just fine.

    Image:pcb-gndplane.PNG

     

    Big pad on the bottom right is the GND pad of the USB connector, as you

    can see an airwire is led to the LQFP pin. There are some "blobs" or

    whatever on both sides of the unconnected pin.

    I think I've clicked just about everything in Eagle, still no-go.

     

    Eagle 6.2.0 Light.

     

     

    Regards

     

    Check the trace size of the polygon that you're using to define the

    ground plane.  It may be that the polygon trace size is too large to make

    the connection to the package.

     

    --

    Tim Wescott

    Control system and signal processing consulting

    www.wescottdesign.com

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I've checked this with QFP144 package and it's still the same so I guess thats more like a program problem than a packages one.

    I've reduced the grid to "finest" setting, no help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    it does the same thing on mine so there has to be somthing wrong with the package.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Yes, tried both of that - current PCB grid is 0.00625inch, and I've tried manually connecting all ground pins without the supply symbol and naming the net 'gnd' - the effect is still the same.

     

    Also, I've put a genuine LQFP-100 part from atmel.lbr (AT91SAM7X128-AU) and connected random pins to GND - the effect is the same:

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    hellow Michal, welcome to the community. have you tried changing the grid size to a smaller size and routing the GND pins of the ic to the usb GND pin in the scematic?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Oh, it got worse. I suspected the package to be of some problem, so I changed it from analog-devices to atmel's LQFP-100 and reconnected all pins. Now it won't even airwire them, so I cant connect them manually. And if the two or more pins are next to each other they are connected properly, only the single ones are left unconnected.