Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) PCB ground plane not connecting to ground pins
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 3807 views
  • Users 0 members are here
Related

PCB ground plane not connecting to ground pins

e14 Contributor
e14 Contributor over 13 years ago

Hello,

 

I did some PCBs with Eagle, so I was quite sure I know it's basics, especially when it comes to ground and power planes.

 

I have a LQFP-100 device with some pins supposed to be connected to ground. I made a ground plane on the top layer, named it GND, same name as the gound net on schematics. Yet the plygon won't connect to the gound pins. I've put right next to the LQFP a different device (USB port) with ground pins as well - those are connected just fine.

image

 

Big pad on the bottom right is the GND pad of the USB connector, as you can see an airwire is led to the LQFP pin. There are some "blobs" or whatever on both sides of the unconnected pin.

I think I've clicked just about everything in Eagle, still no-go.

 

Eagle 6.2.0 Light.

 

 

Regards

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    A side note,

     

    Your isolation seems to be really small. This is the gap between the GND flood and the other, non GND pins. Try setting it to around 10 or 12 mil, to prevent accidental shorts caused by manufacturing errors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Thank you all, indeed it was the problem with polygon trace widh - had to set it to 0 to make it work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Thank you all, indeed it was the problem with polygon trace widh - had to set it to 0 to make it work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Be aware that it is not good practice to use zero width  polygon wires.

    That will make gerber files large. I tried your situation and could get it

    working with 7 mil wires with 8 mil spacing in the DRC.

     

    Warren

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.