Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Plated hole in SMD pad
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 188 subscribers
  • Views 1510 views
  • Users 0 members are here
  • pad
  • library
  • question
Related

Plated hole in SMD pad

e14 Contributor
e14 Contributor over 13 years ago

Hi

 

I've been using eagle for over 10 years. Currently using Eagle 5.12.

 

I am using some smt bottom feed through recepticles from mill max PDFs below.

 

actual part -http://www.mill-max.com/pdf/datasheet/pin_rec_catalog/8874-0-15-01-11-27-10-0.pdf

footprint- http://www.mill-max.com/pdf/datasheet/sockets/388-44-102-11-740799.pdf

 

How do I make a pad with a plated through hole in it's center, without causing an error?

 

Thanks,

Kim S.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    RadioCtrlDWife wrote:

    Hi

     

    I've been using eagle for over 10 years. Currently using Eagle 5.12.

     

    I am using some smt bottom feed through recepticles from mill max

    PDFs below.

     

    actual part

    -http://www.mill-max.com/pdf/datasheet/pin_rec_catalog/8874-0-15-01-11-27-

    10-0.pdf

    footprint-

    http://www.mill-max.com/pdf/datasheet/sockets/388-44-102-11-740799.pdf

     

    How do I make a pad with a plated through hole in it's center,

    without causing an error?

     

    Thanks,

    Kim S.

     

    It's not possible to make that footprint in Eagle without errors

    Eagle Version 6  cannot make it either.

     

     

    Plated holes can only exist if you use a pad the DRILL  of which is  plated

    through.

    A HOLE which is not plated through does not meet your requirements.

    So it seems you need to use a PAD. Alas the DRC will adjust the pad so the

    restring has width and that will spoil your footprint.

     

    So it's back to the hole again.

    You could instruct the board house merge the HOLES and DRILLS files so the

    HOLES are plated through. You could manually do this yourself.

    A ULP would be useful for that. Maybe there is one.

     

    So the package becomes two SMD pads with holes. Alas there will be DRC

    errors that you will need to approve.

     

    I have suggested previously that Eagle needs a  HOLE parameter named 'PTH'.

    If it is 'true' the HOLE is treated as a DRILL, is plated through and the

    signals (pours) don't keep clear of it so the PTH connects to copper. In a

    package this hole/drill would need to be considered part of the SMD /Contact

    and not generate a DRC error.

     

    HTH

    Warren

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    RadioCtrlDWife wrote:

    Hi

     

    I've been using eagle for over 10 years. Currently using Eagle 5.12.

     

    I am using some smt bottom feed through recepticles from mill max

    PDFs below.

     

    actual part

    -http://www.mill-max.com/pdf/datasheet/pin_rec_catalog/8874-0-15-01-11-27-

    10-0.pdf

    footprint-

    http://www.mill-max.com/pdf/datasheet/sockets/388-44-102-11-740799.pdf

     

    How do I make a pad with a plated through hole in it's center,

    without causing an error?

     

    Thanks,

    Kim S.

     

    It's not possible to make that footprint in Eagle without errors

    Eagle Version 6  cannot make it either.

     

     

    Plated holes can only exist if you use a pad the DRILL  of which is  plated

    through.

    A HOLE which is not plated through does not meet your requirements.

    So it seems you need to use a PAD. Alas the DRC will adjust the pad so the

    restring has width and that will spoil your footprint.

     

    So it's back to the hole again.

    You could instruct the board house merge the HOLES and DRILLS files so the

    HOLES are plated through. You could manually do this yourself.

    A ULP would be useful for that. Maybe there is one.

     

    So the package becomes two SMD pads with holes. Alas there will be DRC

    errors that you will need to approve.

     

    I have suggested previously that Eagle needs a  HOLE parameter named 'PTH'.

    If it is 'true' the HOLE is treated as a DRILL, is plated through and the

    signals (pours) don't keep clear of it so the PTH connects to copper. In a

    package this hole/drill would need to be considered part of the SMD /Contact

    and not generate a DRC error.

     

    HTH

    Warren

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks Warren.

     

    Yes, The package looks fine in the libray (I put the pads on a metric grid and the holes on a english grid to avoid the overlap error) until I add it to the board, then the DRC changes the diameter of the holes of the pad within the smd pad, causing the edges of the pads to touch eacother. Of course if I change the DRC setting the rest of the board is affected causing other DRC errors.

     

    The pcb printing house I use typically plates holes, I just want to make sure the holes are connected to the pads correctly. Perhaps I should contact them and confirm this...

     

    Here's a screen shot of what happens when I add the part to a board. Note the board has other violations which are the least of my concerns at the moment. First image is in the library device editor, second image is in board.

    image

     

    Kim S.